This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Btool Error

Part Number: CC2640R2F

Hi Sir,

 At the time of OAD, Btool shows below error 

 OAD Attribute Image Handles Not Found

 I am Using

 Stack 1.4

 CCS 7.4.0

 for OAD I am using the .bin file

 How to Solve Above Error?

Regard's

Toravi

 

 

  • Hi Rohit,

    The BTool Image Header Dialog within BTool will be a good view to use to check the various fields in the image header. Navigate to Over The Air Download pane -> read image file -> image header button. Can you verify that all the fields are populated correctly for your image? 

    If all the image fields appear correct, to gather more information on what could be causing this issue:

    • Can you please provide the full BTool log please?
    • Are you using the off-chip or on-chip?
    • To verify, how was the .bin file generated?
    • Which SDK version of CC2640R2 are you using?

    The following resources may also help with using OAD and BTool:

    Best Regards,

    Jenny