Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG, BOOSTXL-SHARP128
Hello,
Recently I bought a BOOSTXL-SHARP128 (which has a 128*128 Sharp LCD) board to add a LCD Display for a product, the tests were all good and we decided to go with the bigger 400*240 LCD from same manufacturer since we needed a bigger display by our requirements. The 400*240 LCD works good after I changed the display size sin sysconfig for the project. I changed it to 400 as the image below and after that I was able to see tha same displays as per the 128*128 display.
My problem really is that ther upper half of the LCD doesnt persist, It only shows and then it is cleared even if I dont have any clear command running from the app. (If someone needs a video of this issue just let me know and I can show the issue on video directly).
I have looked the forums and some people stated that I may have to increase RAM buffer for the LCD Display Driver or maybe tell the driver that it is now running an 400*240 LCD Display and not the smaller 128*128 but I was not able to manage to do this (I'm quite unexperienced (one year or so) still on TI tools and sysconfig, ccs and CC2642 FW development)
If anyone have any insigh or could help me on this topic I would appreciate really much.
Best Regards and thanks in advance.