Part Number: CC2640R2F
Other Parts Discussed in Thread: UNIFLASH, FLASH-PROGRAMMER
I have created the binary image of the host_test project using the command
${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin ${BuildArtifactFileName} ${BuildArtifactFileBaseName}.bin ${CG_TOOL_ROOT}/bin/armofd ${CG_TOOL_ROOT}/bin/armhex ${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin
After flashing the image to the chip, the CRC is computed and verified which is same as the file CRC.
But when the chip is reset and entered into bootloader , issuing the compute CRC results in CRC that is iifferent than the one computed from previous flashing. Does the flashing is persistent ?
Did I missed any setting in the image ? My CCFG register value is 0xc5ff15c5 --> corresponds to DIO 21.
When the DIO 21 pin is set to high and the BLE_RESET pin is set to high the chip enters into bootloader.
BR
Django