Other Parts Discussed in Thread: LM5155, LM34936, LM5176
Hi,
I am looking to buy an off the shelf boost converter module with the gate drivers built in to test a control mechanism I'm developing. I also need to measure the inductor current and output voltage, and it would be preferable if the sensors were built in too. If the sensors are not built-in, I would need access to the inductor and capacitor to place my own sensors.
Are there any TI products/development boards I could buy off the shelf to help me save time in hardware design and building?
Specs:
Input Voltage: 30V max.
Output Voltage: 72V max.
Switching frequency: capable of switching at 50kHz
Power = 100W (Flexible on this spec)