Part Number: SMARTRF06EBK
Ran into "Failed to load the CPU core driver" message when starting the IAR 8.32.2 debugger using the SmartF06 emulator (TI XDS).
I have re-installed the ti_emupack_setup_9.2.0.00002_win_64.exe also and didn't help.
Below is the IAR debug log:
Tue Mar 23, 2021 12:26:52: IAR Embedded Workbench 8.32.2 (C:\
Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\
bin\armproc.dll)
Tue Mar 23, 2021 12:26:52: Loaded macro file: C:\Program Files (x86)\
IAR Systems\Embedded Workbench 8.2\arm\config\debugger\
TexasInstruments\CC26x0.dmac
Tue Mar 23, 2021 12:26:52: Connecting to TI XDS100v3 ( Probe no:
1220155E ) COM[--/7]
Tue Mar 23, 2021 12:32:16: Fatal error: Failed to load the CPU core
driver Session aborted!
Tue Mar 23, 2021 12:32:16: IAR Embedded Workbench 8.32.2 (C:\
Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\
bin\armproc.dll)