Hi,
Is it possible to detect the angle values of multiple peripherals at the same time in CL-AOA?
I sent the RTLS_CMD_CREATE_SYNC command twice, but the second time it returns a debug message (RTLS Services Error).
HOST >> Central: fe 0e 00 39 09 01 00 00 b1 e7 ee b0 6f 80 00 00 90 01 00 49
HOST << Central: fe 01 00 79 09 00 71
HOST >> Central: fe 0e 00 39 09 01 00 00 46 e7 ee b0 6f 80 00 00 90 01 00 be
HOST << Central: fe 01 00 79 09 00 71
HOST << Central: fe 44 00 59 82 0c 00 00 00 52 54 4c 53 20 53 65 72 76 69 63 65 73 20 45 72 72 6f 72 00 52 54 4c 53 20 53 65 72 76 69 63 65 73 20 43 54 45 20 52 65 71 20 46 61 69 6c 00 c0 78 68 00 28 06 46 00 f0 8e 81 b0 f8 07 00 cb 00 3e
SDK: simplelink_cc13x2_26x2_sdk_4_40_00_44
Regards, Gotoda