Part Number: LAUNCHXL-CC2640R2
Hello,
I am new to using LAUNCHXL-CC2640R2 development kit. I have installed CCS 7.2.0, CCs 10.2.0 and Simple Link SDK 1.40.00.45 in my system. When I tried downloading the image file *oad.bin from BTool, it brought up the attached Connection Handle error.
I tried the following steps:
(1) Built the project in CCS 10.2.0 as the project file is not compatible to 7.2.0
(2) Connected LAUNCHXL-CC2640R2 to my system and opened BTool (available in simplelink SDK 1.40.00.45 tools sub folder)
(3) Established serial port connection in BTool and scanned for the board (Scan was successful)
(4) Established connection after entering the device address under the Discover/Connect tab in BTool
(5) Under OAD tab in BTool, selected the .bin file to be downloaded over the air to the development kit
NOTE: I could see that the Handle has a value of: 0xFFFE, as soon as I scan for development kit from BTool
Also, I am unable to find the simplelink perpheral oad offchip project file that is compatible to be used with CCS 7.2.0. It will be great if someone could guide me in finding the example projects that are compatible with CCS 7.2.0 as this is the version required for my project.
Best Regards,
Nandhini Jayapandian