Part Number: CC2652P
Hi, I use CC2652P, simplelink_cc13x2_26x2_sdk_4_40_04_04, CCS10.2.
My application is based on dmm example as below:

In the .opts file as below:

There are some predefined symbols.
1, there is a CC13XX symbol, do I need to change it to or add a CC2652 symbol since there are such codes as below, and my target is based on CC2652P

2, there is an xAUTO_START symbol which means AUTO_START is disabled, what does this AUTO_START mean? Do I need to make it enabled by deleting 'x'?
3,there is a xPOWER_MEAS symbol, what does this POWER_MEAS mean, do I need to enable it?
Thank you.