This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Project build options when CC2642 migration to the CC2652 takes place

Part Number: CC2652R
Other Parts Discussed in Thread: CC2642R, SYSCONFIG

Hello everyone! 

I am sorry, but can anyone approve that CC2642R and CC2652R both have the same HAL ? In other words - are there any other differences except the BLE vs BL+802.15.4 ?

I am porting my project from the CC2642R to the CC2652R and I need to be sure, that HAL is the same, memory map and register's map too.

I have checked the datasheets and the CC26X2 -manual - but there are any words about the HAL or any other difference between the CC2652R and  the CC2642R. Their pinouts are identical, but what is 'under the cover' ? Maybe all is OK, but I need to be sure - not to fail or burn the chip or break the BL support.

Thanks a lot.

P.S. I have tried the SysConfig chip switching and it switches a lot - from the PIN numbers and so on... Can anyone clear up the migration from the CC2642 to CC2652 building options ? The target config I have already solved.

Thanks a lot.