Part Number: CC2640R2F
Hello,
I have a custom board. I am trying to evaluate impact to RSSI from different battery voltages using SmartRF Studio.
I've adapted a LAUNCHXL board to be the programming interface for the board and it works great.
When I remove power from Vin and reconnect the custom board to the lauchpad, the device boots up.
The only electrical connections are through pogo pins that connect to TMSC, TCKC, TDO, TDI and RESET.
I get ~2.8v measured on my custom board Vin pins.
Am I getting leakage through TCKC and its powering the device?
TCKC is around 3.3v
RESET is less then 2.8v
And if I am getting leakage through there, how do I mitigate the system powering up through that pin.
I appreciate the help on this head scratcher.