Other Parts Discussed in Thread: CC1352R
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tried SimpleLink also. DId not work with this app either.
Thanks for the response though.
What SDK version are you using? There has been a known issue with the accelerometer that was fixed in SDK4.20:
https://dev.ti.com/tirex/content/simplelink_cc13x2_26x2_sdk_4_20_00_35/changelog.html#fixed-issues
(DMM-886)
Also see the following post:
Siri
Current latest CC13x2/CC26x2 SDK is Version: 5.10.00.48. What do you mean SDK v5.7.5 (Build 86) and where do you download it?
CC26x2
I am referring to Simple Link app v5.7.5 as suggested by you above on Google Play store.
Following steps for "Your LaunchPad's Out of Box Experience demo"
Have you updated the code on the LP with the code from the latest SDK (5.10)?
As I wrote in the first post, there has been a bug on the LPSTK regarding the Acc. I am not sure with SDK is used for the code that comes with the LPSTK, so please update with the latest code from the simplelink_cc13x2_26x2_sdk_5_10_00_48 SDK.
Siri
I can confirm multi_sensor example in SDK 5.10 can see accelerator data without problem on my iPhone 7 plus.
Yes, works for me also for other piece I have. Therefore I suspect the problem is with this one device.
Do you mean that you have two LPSTK-CC1352R, one works and another doesn’t with the same software? If so, I would say this might be hardware broken.