Other Parts Discussed in Thread: MSP432E401Y, CC2564, CC2564C, MSP-EXP432E401Y, CC2564MODNEM,
Hi,
I am using MSP432E401Y with CC2564MODA Bluetooth module. At this moment I am able to communicate with the module using the bluetopia stack.
I am calling InitializeApplication() function successfully we can find on SPPDemo.c file (\Samples\SPPDemo). After initialize the Bluetooth Stack, I am able to open the SPP server using OpenServer() and I call periodically BTPS_ProcessScheduler(). But at this point, my device is not advertising neither accepts Bluetooth connections.
When running my code, this output is provided on the debug console:
OpenStack().
Bluetooth Stack ID: 1
Device Chipset: 4.1
BTPS Version : 4.0.3.0
Project Type : 6
FW Version : 7.26
LOCAL BD_ADDR: CC:78:AB:7D:84:B8
Local Device Name(): MY_BTH_DEVICE
Server Opened: 1.
All mode are OK when I query for the current mode parameters using GAP_Query_Connectability_Mode(), GAP_Query_Discoverability_Mode() and GAP_Query_Pairability_Mode().
Can someone tell me what procedures should I take to detect any anomalies?
Best Regards
Nuno Dias
----------------------------------------------------------
Bellow some code snippets I am extracted from bluetopia stack samples:
int bluetooth_init(void)int bluetooth_init(void) {
DEBUG_MSG("");
int Result;
BTPS_Initialization_t BTPS_Initialization;
HCI_DriverInformation_t HCI_DriverInformation;
HCI_HCILLConfiguration_t HCILLConfig;
HCI_Driver_Reconfigure_Data_t DriverReconfigureData;
/* Configure the hardware for its intended use. */
HAL_ConfigureHardware();
/* Configure the UART Parameters nd Initialize the Bluetooth Stack. */
HCI_DRIVER_SET_COMM_INFORMATION(&HCI_DriverInformation, 1, HAL_HCI_UART_MAX_BAUD_RATE, cpHCILL_RTS_CTS);
HCI_DriverInformation.DriverInformation.COMMDriverInformation.InitializationDelay = 100;
/* Set up the application callbacks. */
BTPS_Initialization.GetTickCountCallback = getTickCountCallback;
BTPS_Initialization.MessageOutputCallback = msgOutputCallback;
/* Initialize the application. */
Result = InitializeApplication(&HCI_DriverInformation, &BTPS_Initialization);
if (Result > 0) {
/* Save the Bluetooth Stack ID. */
BluetoothStackID = (unsigned int)Result;
Result = OpenServer(SPP_PORT_NUMBER_MINIMUM);
} else {
DisplayFunctionError("Initialize the application", Result);
}
int InitializeApplication(HCI_DriverInformation_t *HCI_DriverInformation, BTPS_Initialization_t *BTPS_Initialization)
/* The following function is used to initialize the application */
/* instance. This function should open the stack and prepare to */
/* execute commands based on user input. The first parameter passed */
/* to this function is the HCI Driver Information that will be used */
/* when opening the stack and the second parameter is used to pass */
/* parameters to BTPS_Init. This function returns the */
/* BluetoothStackID returned from BSC_Initialize on success or a */
/* negative error code (of the form APPLICATION_ERROR_XXX). */
int InitializeApplication(HCI_DriverInformation_t *HCI_DriverInformation, BTPS_Initialization_t *BTPS_Initialization)
{
int ret_val = APPLICATION_ERROR_UNABLE_TO_OPEN_STACK;
/* Initialize some defaults. */
SerialPortID = 0;
bthRole = BTH_ROLE_NONE;
NumberofValidResponses = 0;
/* Next, makes sure that the Driver Information passed appears to be */
/* semi-valid. */
if((HCI_DriverInformation) && (BTPS_Initialization))
{
/* Try to Open the stack and check if it was successful. */
if(!OpenStack(HCI_DriverInformation, BTPS_Initialization))
{
/* The stack was opened successfully. Now set some defaults. */
/* First, attempt to set the Device to be Connectable. */
ret_val = SetConnect();
/* Next, check to see if the Device was successfully made */
/* Connectable. */
if(!ret_val)
{
/* Now that the device is Connectable attempt to make it */
/* Discoverable. */
ret_val = SetDisc();
/* Next, check to see if the Device was successfully made */
/* Discoverable. */
if(!ret_val)
{
/* Now that the device is discoverable attempt to make it*/
/* pairable. */
ret_val = SetPairable();
if(!ret_val)
{
/* Attempt to register a HCI Event Callback. */
ret_val = HCI_Register_Event_Callback(BluetoothStackID, HCI_Event_Callback, (unsigned long)NULL);
if(ret_val > 0)
{
/* Assign a NULL BD_ADDR for comparison. */
ASSIGN_BD_ADDR(NullADDR, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00);
/* Save the maximum supported baud rate. */
MaxBaudRate = (DWord_t)(HCI_DriverInformation->DriverInformation.COMMDriverInformation.BaudRate);
/* Return success to the caller. */
ret_val = (int)BluetoothStackID;
}
else
DisplayFunctionError("HCI_Register_Event_Callback()", ret_val);
}
else
DisplayFunctionError("SetPairable", ret_val);
}
else
DisplayFunctionError("SetDisc", ret_val);
}
else
DisplayFunctionError("SetDisc", ret_val);
/* In some error occurred then close the stack. */
if(ret_val < 0)
{
/* Close the Bluetooth Stack. */
CloseStack();
}
}
else
{
/* There was an error while attempting to open the Stack. */
Display(("Unable to open the stack.\r\n"));
}
}
else
ret_val = APPLICATION_ERROR_INVALID_PARAMETERS;
return(ret_val);
}