This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Programming CC2650

Part Number: CC2650

I have to program a device with CC2650MODA. But I don't have that device yet. I have a cc2650 launchpad. So, I thought about creating a code with cc2650 and use that code for the device with cc2650MODA. I have started to program cc2650 with BLE_SDK_2_02_05_02.

  • Is both CC2650 launchpad and cc2650MODA uses the same SDK? I want to create a code from the simple peripheral example program.
  • Hi,

    The same SDK can be used for CC2650 launchpad and CC2650MODA. That being both do not use the exact same CC2650 package, so you will be required to through a short porting process (the procedure is described here).

    In summary, this is a good idea to start developing on CC2650 launchpad until you receive the CC2650MODA.

    I hope this will help,

    Regards,