Part Number: CC2652R
Other Parts Discussed in Thread: TPS62740, ,
I've used a similar configuration for the CC2652RB based mainly on the "Using the Wireless SimpleLink CC26xx in External Regulator Mode With the TPS62740" app note as well as the "CC2650EM-4XS-Ext_Reg_2_0_0" reference design. I need to run a new board but I'm being forced to use the CC2652R and TPS62231 due to the chip shortage. I just want to ensure the inductor recommendation on the regulator and DCOUPL capacitance is suited for upgrading to the CC2652RB when it becomes available again?