Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640, CC2650
Hi Sir / Madam,
I am using IAR IDE and rearranging the file structure of CC2460R2.
One of the example file inside "blestack" folder : D:\ti\simplelink_cc2640r2_sdk_1_00_00_22\examples\rtos\CC2640R2_LAUNCHXL\blestack ,
is taken out and place it into "ti" folder : D:\ti .
So when I compile it, it has error, such as : Cannot find input file ..... .
May I know how can I modify the " peripheral_example.custom_argvars" so that it can compile successfully ?
My file structure is :
D:\Project\Example_peripheral\Example_peripheral
D:\Project\Example_peripheral\simplelink_cc2640r2_sdk_1_00_00_22
D:\Project\Example_peripheral\xdctools_3_32_01_22_core
Thank you very much.
Your effort is very much appreciated.
Cheers,
KF