This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Angle of arrival using RTLS Ui

Part Number: LAUNCHXL-CC26X2R1

Hello,

I have a problem.

I am using the following hardware:

* LAUNCHXL-CC26X2R1 (x2)

* BOOSTXL-AOA (x1)

I am adopting Option 3 in Task 1 - Running the AoA application in the SLA Bluetooth Low Energy Angle of Arrival (AoA): http://dev.ti.com/tirex/explore/node?node=AHYhhuDNTaRXzkOlahOlvA__pTTHBmu__LATEST

I have successfully programmed both (master and slave) boards. And obviously I am using the simplelink_cc13x2_26x2_sdk_3_40_00_02.

Everything runs perfectly fine except when I go to the AoA configurations in the RTLS UI that doesn't work if I choose the option of using both antenna's. I get the following error output:

I tried doing what is recommended and I arrived here in the E2E asking this question.

I'd appreciate any help since I am blocked for two days now.

Regards,