Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Now I add UART debugging to AOA example, but when I Emulator it, I find that UART is not loaded every time, which is why
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Now I add UART debugging to AOA example, but when I Emulator it, I find that UART is not loaded every time, which is why
Hi,
I am assigning an expert to comment on this for you. Also, which SDK version are you using for your environment?
Regards,
Michael
OK, but,Why can't my UART send data after sending it once,I found that the program was stuck in hwip_disable when I was debugging one step HwiP。i need please help,i need please help , I have been adding UART to AOA for 1 month. But it didn't work. i use cc26x2r1 lunch pad, SDK is simplelink_cc13x2_26x2_sdk_4_10_00_78.
Hi,
Have you used SysConfig to add the second UART? If not done, please do so. (If needed, here is a lab to help)
Then you have to use the new UART and properly open (UART_open) it before your call UART_write. You can consult the documentation in order to get some examples to configure the UART and to use it. I recommend to use the UART in Callback mode and to run some tests (in order to see if the UART is properly configured) outside of the rtls example.
I hope this will help,
Regards,
yeah,I've opened UART_ open,so I found out in BIOS_ Start () before calling uart_ Write is bound to get stuck,I've found that this is true for any TI-RTOS based example,But I found that with the TI-RTOS example, I output system_Printf () is enough,so i just redirect UART to system_printf,it's ok.