Part Number: LAUNCHXL-CC26X2R1
Dear E2E
I have problems launching RTLS Agent:



I have followed all the recommendations in the Readme
Now parameters of system is below:
Windows 7 Pro SP1
Python 3.7.0
Code Composer Studio Version: 10.2.0.00009
I used SDK's : First use - simplelink_cc13x2_26x2_sdk_4_40_04_04
then simplelink_cc13x2_26x2_sdk_4_40_00_44
About a log string "...UnicodeDecodeError: 'utf-8' codec can't decode byte 0x88 in position 1: invalid start byte ..."
All resourses in project - UTF-8 encoding

Please help me