Part Number: BOOSTXL-AOA
greetings,
Is it possible to mining the collect IQ data for environment sensing task ? Clément like monitor human activity. As we know as human move, the channel state changes, and the received the IQ data may change to anther waveform.
To this end, I come up with and complete these:
1. save down the timestep
2. control the collection time and sample eate
3. lift the TX power a bit for better SNR
4. keep the channel as constant.
While the point I have not figure out is, which is also mention in post [control the Transmitter (the slave node) to send same message]
1. control the send signal as fixed
Does these make sense, is there anything else I need to take care with? I might concern about that the SNR is too low that make IQ data noisy and less qualified.
Best.
Jet