Part Number: CC8531
I'm wondering if anyone else have stumbled on the same issue that I have with programming the CC85xx devices?
I'm using the CC Debugger and PurePath Wireless Console and for the moment only CC8531.
So far I've built 4 boards and all were detected by both the CC Debugger and PPWC. Flashing the chip appears to be successful and the status LED on the CC8531 board is flashing indicating "alone mode", but then none of the boards can be flashed again. CC Debugger does at this stage detect the connected CC8531 (green LED) but in PPWC it stays as disconnected.
I have tried with and without a 56k pull-up resistor on the reset pin but that makes no difference either way.
Any ideas would be greatly appreciated
Thanks,
Mattias