This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF430CL331H: can`t transmitte

Part Number: RF430CL331H


In the test of using rf430cl331h chip, we found that only 249 bytes can be transmitted. The chip manual says that 3K bytes can be transmitted. What should I do if I want to transmit more than 250 bytes?

Moreover, the application example introduces that the maximum data that can be transmitted is limited by the master MCU, and 40K bytes can be used for sending in the instance.

Whether there are instances available.