15693协议,使用260100指令,请求读取标签UID,标签已经返回数据(可以再OOK/ASK引脚看到信号),但是TRF7964A的FIFO里面没有数据
IRQ Status Register (0x0C),这个中断寄存器里面已经收到0x40标志(IRQ set due to RX start),并且等到IRQ引脚有效,再次去读取FIFO长度寄存器,显示FIFO长度数据是0
这个情况不是每次都能出现,但是一旦出现后,通过软件复位TRF7964A,没有效果,情况依然存在
IRQ Status Register (0x0C)中断寄存器中
CRC error
Parity error
Byte framing or EOF error
Collision error
No response time interrupt
这些标志位都是0