Part Number: CC1352R
Other Parts Discussed in Thread: SYSCONFIG
Hi!
My environment:
Custom Board CC1352R1
SDK: 5.20.0.52
SYSCONFIG: 1.8.2
Problem:
I have custom board based on CC1352R1. I want to set external LF Clock Source but I can't get it work.
I changed LF Clock Source in syscfg file and set external DIO as I have on my board, but all the time program stops in Board_init on PIN_close function.
I can see that problem is with PIN_remove function, it fails on condition because handle is NULL and returns PIN_NO_ACCESS.
I double checked signal from external oscillator and it's fine. I also tried to use different SDKs (5.20.0.52, 5.10.0.48 and 4.20.1.04) and different Sysconfigs (1.8.2, 1.8.0 and 1.6.0).
What can I do to make it works? Is it some kind of bug?