Other Parts Discussed in Thread: REMOTI
Hi,
Basically, in RF4CE, target determines which frequency bands (MAC ch15, 20 or 25) the network will operate in ( ->called: frequency agility).
Understand that, In RemoTI this 'frequency agility' feature can be disabled in the 'Target', to enable single channel pairing (by selecting/setting which channel we want the target to operate in). In this case, 'Controller' will send out discovery frames in all three channels, but it will only be paired in the Target's frequency during the pairing/discovery.
For testing purposes, 3 Controllers is going to be paired with 3 different Targets (in the same room), to constitute one single channel for each succesful pairing; means all three pairing MUST be in three different channels. eg:
* CONTROLLER 1 paired to TARGET 1 at ch.15.
* CONTROLLER 2 paired to TARGET 2 at ch.20.
* CONTROLLER 3 paired to TARGET 3 at ch.25.
[Q1]: Is it possible to acheive the above scenario (with RemoTI v1.2.x) ?
[Q2]: If possible, please advice how to do it ? What steps need to be done (on the Controller side) ?
Thank you in advance.
Best Regards,
William