Part Number: CC2500
Hi,
I'm trying to capture a proprietary 2.4g signal. I can see CC2500 is a close match for my signal but there are a few problems in my way;
-My signal is 25 byte, 96 kbps on 2.4ghz frequency, FSK modulation. The signal swings between ±500khz. SmartRF studio settings is giving me a maximum value of 405khz chanel spacing. If I leave it as 405, can i still catch this RF signal?
-My signal starts with a preamble of FAAAAAAA and 25 byte value, but CC2500 preamble is AAAA according to the datasheet. Can i set this preamble on the cc2500? If i cant, is CC2500 able to ignore the first byte of the signal and act as this is a 24byte signal which starts with AAAA?
My ultimate question is if I cant use this chip, are there any alternative recommendations that is able to catch this signal?