Other Parts Discussed in Thread: TPS61241,
Hi Team,
I am using TRF7970ARHBT in one of our projects.
I am planning to connect the VIN pin directly to the battery (4.2V maximum) when the USB in is not available and 5V from the USB when it is available.
My MCU is 3.3V logic.
The VDD_X pin cannot be configured to a 3.3V in my case (according to tables 6-1 and 6-2).
I am planning to provide a 3.3V supply from an external regulator to the VDD_IO pin so that my communication with the MCU will be 3.3V logic in that case, can I left the theVDD_X pin unconnected or can I terminate it with proper decoupling.
From my understanding from a brief reading of the datasheet, VDD_X is the voltage with which the digital I/O takes place, and if I configure it to 3.3V and connect it to VDD_IO I'll not need an external 3.3V regulator. If so during power-up what is the voltage at the VDD_X pin?. If that voltage is higher than 3.3V logic my MCU is gonna damage.
Also, the voltage at the VDD_X, VDD_RF, and VDD_A are programmable, to what value do I need to configure these regulators to get the optimum performance?.
I am planning to use a power switch to disconnect the chip from the battery, the pin VIN will be disconnected, is there any problem when VIN is not power and the pin VDD_IO is powered to 3.3V
The TRF7970ARHBT is not available on Mouser or Digikey.