This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: Design

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: ADS1293, CC2640, TIDA-00096, CCSTUDIO

Dear Texas Instrument, 
in TIDA-00096  reference design, we would like to see where the parameter R1 for the ADS1293 is set along with the R2 and R3. The ODR is defined by fs/ (R1.R2.R3).  Also, what is your suggestion to efficiently remap the DIOs when porting from cc2640 to MODACC2650? Further more, it  is not clear how these DIOs are addressed  or called in the CCS code. Please clarify. Also, is  the debugger on the launchpad cJATG so that we do not need the DTI and the DTO?  Thank you!