This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: TRF7970A RX event with 0 bytes in the count register

Part Number: TRF7970A

Hi Helfried Vollbrecht

Here is the signal capture for the TRF7970A ticket. Can you please review and see if you see any problem with the register values or SPI timings?

https://www.dropbox.com/s/33jhb8vkc1ky4wl/trf7970_13mhz_issue_caputure_11112021.sal?dl=0

-------------- ORIGINAL TICKET IS BELOW ----

Hello,

I am testing a custom 13mhz RFID reader board using TRF7970A and based on the reference design. (I can share the schematic on a private message if needed).

I am using the demo code on sloc297c , on Nordic Nrf53 platform, using SPI connected to the TRF7970A.

As far as RF, I can see 23v-24v peak to peak on the antenna test point. I can also see the clean 13mhz tone on the scope when the chip act as a reader.

The card responds when I keep the card on the antenna board.

But when I get the RX_COMPLETE event is reported, in trf79xxa.c -> void TRF79xxA_processIRQ(uint8_t* pui8IrqStatus), -> TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS) always returns 0 bytes in FIFO.

I have the complete SPI transaction logs here... Please note "spi-tx" is just single spi write transaction.  "spi-tx-tx" followed by "spi-tx-rx" is a single transaction of write+read.

See the RX_COMPLETE  marked in Yellow. The next 

[2021-09-29 08:18:24.661] RX_COMPLETE
[2021-09-29 08:18:24.661] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:24.661] spi-tx-rx: 0000 .. << Supposed to have a valid FIFO byte count instead of Zero.

Can you please see if my initialization sequence is correct and any idea why the receive bytes count always zero? 

[2021-09-29 08:18:20.797]
[2021-09-29 08:18:20.797] ****************************************************************
[2021-09-29 08:18:20.835] * Compiled on: Sep 28 2021 18:49:26
[2021-09-29 08:18:20.835] ****************************************************************
[2021-09-29 08:18:20.835] Bootup OK
[2021-09-29 08:18:23.343] spi-tx: 83 .
[2021-09-29 08:18:23.724] spi-tx: 80 .
[2021-09-29 08:18:23.724] spi-tx: 8f .
[2021-09-29 08:18:23.724] spi-tx: 0981 ..
[2021-09-29 08:18:23.724] spi-tx: 0b80 ..
[2021-09-29 08:18:23.724] spi-tx: 1800 ..
[2021-09-29 08:18:23.724] spi-tx-tx: 4000 @.
[2021-09-29 08:18:23.724] spi-tx-rx: 0001 ..
[2021-09-29 08:18:23.724] init reg 00 = 01
[2021-09-29 08:18:23.724] spi-tx-tx: 4100 A.
[2021-09-29 08:18:23.724] spi-tx-rx: 0021 .!
[2021-09-29 08:18:23.724] init reg 01 = 21
[2021-09-29 08:18:23.724] spi-tx-tx: 4200 B.
[2021-09-29 08:18:23.724] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.724] init reg 02 = 00
[2021-09-29 08:18:23.724] spi-tx-tx: 4300 C.
[2021-09-29 08:18:23.724] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.724] init reg 03 = 00
[2021-09-29 08:18:23.724] spi-tx-tx: 4400 D.
[2021-09-29 08:18:23.724] spi-tx-rx: 00c1 ..
[2021-09-29 08:18:23.724] init reg 04 = C1
[2021-09-29 08:18:23.726] spi-tx-tx: 4500 E.
[2021-09-29 08:18:23.726] spi-tx-rx: ffc1 ..
[2021-09-29 08:18:23.726] init reg 05 = C1
[2021-09-29 08:18:23.726] spi-tx-tx: 4600 F.
[2021-09-29 08:18:23.726] spi-tx-rx: ff00 ..
[2021-09-29 08:18:23.726] init reg 06 = 00
[2021-09-29 08:18:23.726] spi-tx-tx: 4700 G.
[2021-09-29 08:18:23.726] spi-tx-rx: 000e ..
[2021-09-29 08:18:23.726] init reg 07 = 0E
[2021-09-29 08:18:23.726] spi-tx-tx: 4800 H.
[2021-09-29 08:18:23.726] spi-tx-rx: 0007 ..
[2021-09-29 08:18:23.726] init reg 08 = 07
[2021-09-29 08:18:23.726] spi-tx-tx: 4900 I.
[2021-09-29 08:18:23.726] spi-tx-rx: 0081 ..
[2021-09-29 08:18:23.726] init reg 09 = 81
[2021-09-29 08:18:23.726] spi-tx-tx: 4a00 J.
[2021-09-29 08:18:23.726] spi-tx-rx: 0010 ..
[2021-09-29 08:18:23.726] init reg 0a = 10
[2021-09-29 08:18:23.726] spi-tx-tx: 4b00 K.
[2021-09-29 08:18:23.726] spi-tx-rx: 0080 ..
[2021-09-29 08:18:23.727] init reg 0b = 80
[2021-09-29 08:18:23.727] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:23.727] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.727] init reg 0c = 00
[2021-09-29 08:18:23.727] spi-tx-tx: 4d00 M.
[2021-09-29 08:18:23.727] spi-tx-rx: 003e .>
[2021-09-29 08:18:23.727] init reg 0d = 3E
[2021-09-29 08:18:23.727] spi-tx-tx: 4e00 N.
[2021-09-29 08:18:23.727] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.727] init reg 0e = 00
[2021-09-29 08:18:23.727] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:23.727] spi-tx-rx: 0040 .@
[2021-09-29 08:18:23.727] init reg 0f = 40
[2021-09-29 08:18:23.727] spi-tx-tx: 5000 P.
[2021-09-29 08:18:23.727] spi-tx-rx: ff00 ..
[2021-09-29 08:18:23.727] init reg 10 = 00
[2021-09-29 08:18:23.727] spi-tx-tx: 5100 Q.
[2021-09-29 08:18:23.727] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.727] init reg 11 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5200 R.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 12 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5300 S.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 13 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5400 T.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 14 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5500 U.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 15 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5600 V.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 16 = 00
[2021-09-29 08:18:23.737] spi-tx-tx: 5700 W.
[2021-09-29 08:18:23.737] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.737] init reg 17 = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5800 X.
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 18 = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5900 Y.
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 19 = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5a00 Z.
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 1a = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5b00 [.
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 1b = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 1c = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5d00 ].
[2021-09-29 08:18:23.863] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.863] init reg 1d = 00
[2021-09-29 08:18:23.863] spi-tx-tx: 5e00 ^.
[2021-09-29 08:18:23.864] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.864] init reg 1e = 00
[2021-09-29 08:18:23.864] spi-tx-tx: 5f00 _.
[2021-09-29 08:18:23.864] spi-tx-rx: 0000 ..
[2021-09-29 08:18:23.864] init reg 1f = 00
[2021-09-29 08:18:23.864] spi-tx: 0001 ..
[2021-09-29 08:18:24.053] spi-tx: 83 .
[2021-09-29 08:18:24.168] spi-tx: 80 .
[2021-09-29 08:18:24.168] spi-tx: 8f .
[2021-09-29 08:18:24.168] spi-tx: 0981 ..
[2021-09-29 08:18:24.168] spi-tx: 0b80 ..
[2021-09-29 08:18:24.168] spi-tx: 1800 ..
[2021-09-29 08:18:24.168] spi-tx: 0002 ..
[2021-09-29 08:18:24.168] spi-tx: 99 .
[2021-09-29 08:18:24.168] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:24.168] spi-tx-rx: 0040 .@
[2021-09-29 08:18:24.168] spi-tx: 83 .
[2021-09-29 08:18:24.168] spi-tx: 80 .
[2021-09-29 08:18:24.168] spi-tx: 8f .
[2021-09-29 08:18:24.168] spi-tx: 0981 ..
[2021-09-29 08:18:24.168] spi-tx: 0b80 ..
[2021-09-29 08:18:24.168] spi-tx: 1800 ..
[2021-09-29 08:18:24.168] spi-tx: 0021 .!
[2021-09-29 08:18:24.168] spi-tx: 010c ..
[2021-09-29 08:18:24.168] spi-tx: 0980 ..
[2021-09-29 08:18:24.168] spi-tx: 1403 ..
[2021-09-29 08:18:24.168] spi-tx: 1800 ..
[2021-09-29 08:18:24.168] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:24.262] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.262] spi-tx-rx: 0080 ..
[2021-09-29 08:18:24.262] spi-tx: 8f .
[2021-09-29 08:18:24.262] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.262] spi-tx-rx: 0040 .@
[2021-09-29 08:18:24.262] RX_COMPLETE
[2021-09-29 08:18:24.262] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:24.262] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.262] spi-tx: 8f .
[2021-09-29 08:18:24.262] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.262] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.262] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.262] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.262] spi-tx: 0001 ..
[2021-09-29 08:18:24.262] spi-tx: 0001 ..
[2021-09-29 08:18:24.453] spi-tx: 83 .
[2021-09-29 08:18:24.567] spi-tx: 80 .
[2021-09-29 08:18:24.567] spi-tx: 8f .
[2021-09-29 08:18:24.567] spi-tx: 0981 ..
[2021-09-29 08:18:24.567] spi-tx: 0b80 ..
[2021-09-29 08:18:24.567] spi-tx: 1800 ..
[2021-09-29 08:18:24.567] spi-tx: 0002 ..
[2021-09-29 08:18:24.567] spi-tx: 99 .
[2021-09-29 08:18:24.567] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:24.567] spi-tx-rx: 0040 .@
[2021-09-29 08:18:24.567] spi-tx: 83 .
[2021-09-29 08:18:24.567] spi-tx: 80 .
[2021-09-29 08:18:24.567] spi-tx: 8f .
[2021-09-29 08:18:24.567] spi-tx: 0981 ..
[2021-09-29 08:18:24.567] spi-tx: 0b80 ..
[2021-09-29 08:18:24.567] spi-tx: 1800 ..
[2021-09-29 08:18:24.567] spi-tx: 0021 .!
[2021-09-29 08:18:24.567] spi-tx: 010c ..
[2021-09-29 08:18:24.567] spi-tx: 0980 ..
[2021-09-29 08:18:24.567] spi-tx: 1403 ..
[2021-09-29 08:18:24.567] spi-tx: 1800 ..
[2021-09-29 08:18:24.567] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:24.661] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.661] spi-tx-rx: 0080 ..
[2021-09-29 08:18:24.661] spi-tx: 8f .
[2021-09-29 08:18:24.661] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.661] spi-tx-rx: 0040 .@
[2021-09-29 08:18:24.661] RX_COMPLETE
[2021-09-29 08:18:24.661] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:24.661] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.661] spi-tx: 8f .
[2021-09-29 08:18:24.661] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.661] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.661] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:24.661] spi-tx-rx: 0000 ..
[2021-09-29 08:18:24.661] spi-tx: 0001 ..
[2021-09-29 08:18:24.661] spi-tx: 0001 ..
[2021-09-29 08:18:24.852] spi-tx: 83 .
[2021-09-29 08:18:24.967] spi-tx: 80 .
[2021-09-29 08:18:24.967] spi-tx: 8f .
[2021-09-29 08:18:24.967] spi-tx: 0981 ..
[2021-09-29 08:18:24.967] spi-tx: 0b80 ..
[2021-09-29 08:18:24.967] spi-tx: 1800 ..
[2021-09-29 08:18:24.967] spi-tx: 0002 ..
[2021-09-29 08:18:24.967] spi-tx: 99 .
[2021-09-29 08:18:24.967] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:24.967] spi-tx-rx: 0040 .@
[2021-09-29 08:18:24.967] spi-tx: 83 .
[2021-09-29 08:18:24.967] spi-tx: 80 .
[2021-09-29 08:18:24.967] spi-tx: 8f .
[2021-09-29 08:18:24.967] spi-tx: 0981 ..
[2021-09-29 08:18:24.967] spi-tx: 0b80 ..
[2021-09-29 08:18:24.967] spi-tx: 1800 ..
[2021-09-29 08:18:24.967] spi-tx: 0021 .!
[2021-09-29 08:18:24.967] spi-tx: 010c ..
[2021-09-29 08:18:24.967] spi-tx: 0980 ..
[2021-09-29 08:18:24.967] spi-tx: 1403 ..
[2021-09-29 08:18:24.967] spi-tx: 1800 ..
[2021-09-29 08:18:24.967] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:25.060] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.060] spi-tx-rx: 0080 ..
[2021-09-29 08:18:25.060] spi-tx: 8f .
[2021-09-29 08:18:25.060] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.060] spi-tx-rx: 0040 .@
[2021-09-29 08:18:25.060] RX_COMPLETE
[2021-09-29 08:18:25.060] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:25.060] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.060] spi-tx: 8f .
[2021-09-29 08:18:25.060] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.060] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.060] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.060] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.060] spi-tx: 0001 ..
[2021-09-29 08:18:25.060] spi-tx: 0001 ..
[2021-09-29 08:18:25.251] spi-tx: 83 .
[2021-09-29 08:18:25.366] spi-tx: 80 .
[2021-09-29 08:18:25.366] spi-tx: 8f .
[2021-09-29 08:18:25.366] spi-tx: 0981 ..
[2021-09-29 08:18:25.366] spi-tx: 0b80 ..
[2021-09-29 08:18:25.366] spi-tx: 1800 ..
[2021-09-29 08:18:25.366] spi-tx: 0002 ..
[2021-09-29 08:18:25.366] spi-tx: 99 .
[2021-09-29 08:18:25.366] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:25.366] spi-tx-rx: 0040 .@
[2021-09-29 08:18:25.366] spi-tx: 83 .
[2021-09-29 08:18:25.366] spi-tx: 80 .
[2021-09-29 08:18:25.366] spi-tx: 8f .
[2021-09-29 08:18:25.366] spi-tx: 0981 ..
[2021-09-29 08:18:25.366] spi-tx: 0b80 ..
[2021-09-29 08:18:25.366] spi-tx: 1800 ..
[2021-09-29 08:18:25.366] spi-tx: 0021 .!
[2021-09-29 08:18:25.366] spi-tx: 010c ..
[2021-09-29 08:18:25.366] spi-tx: 0980 ..
[2021-09-29 08:18:25.366] spi-tx: 1403 ..
[2021-09-29 08:18:25.366] spi-tx: 1800 ..
[2021-09-29 08:18:25.366] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:25.460] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.460] spi-tx-rx: 0080 ..
[2021-09-29 08:18:25.460] spi-tx: 8f .
[2021-09-29 08:18:25.460] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.460] spi-tx-rx: 0040 .@
[2021-09-29 08:18:25.460] RX_COMPLETE
[2021-09-29 08:18:25.460] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:25.460] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.460] spi-tx: 8f .
[2021-09-29 08:18:25.460] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.460] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.460] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.460] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.460] spi-tx: 0001 ..
[2021-09-29 08:18:25.460] spi-tx: 0001 ..
[2021-09-29 08:18:25.650] spi-tx: 83 .
[2021-09-29 08:18:25.765] spi-tx: 80 .
[2021-09-29 08:18:25.765] spi-tx: 8f .
[2021-09-29 08:18:25.765] spi-tx: 0981 ..
[2021-09-29 08:18:25.765] spi-tx: 0b80 ..
[2021-09-29 08:18:25.765] spi-tx: 1800 ..
[2021-09-29 08:18:25.765] spi-tx: 0002 ..
[2021-09-29 08:18:25.765] spi-tx: 99 .
[2021-09-29 08:18:25.765] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:25.765] spi-tx-rx: 0040 .@
[2021-09-29 08:18:25.765] spi-tx: 83 .
[2021-09-29 08:18:25.765] spi-tx: 80 .
[2021-09-29 08:18:25.765] spi-tx: 8f .
[2021-09-29 08:18:25.765] spi-tx: 0981 ..
[2021-09-29 08:18:25.765] spi-tx: 0b80 ..
[2021-09-29 08:18:25.765] spi-tx: 1800 ..
[2021-09-29 08:18:25.765] spi-tx: 0021 .!
[2021-09-29 08:18:25.765] spi-tx: 010c ..
[2021-09-29 08:18:25.765] spi-tx: 0980 ..
[2021-09-29 08:18:25.765] spi-tx: 1403 ..
[2021-09-29 08:18:25.765] spi-tx: 1800 ..
[2021-09-29 08:18:25.765] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:25.859] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.859] spi-tx-rx: 0080 ..
[2021-09-29 08:18:25.859] spi-tx: 8f .
[2021-09-29 08:18:25.859] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.859] spi-tx-rx: 0040 .@
[2021-09-29 08:18:25.859] RX_COMPLETE
[2021-09-29 08:18:25.859] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:25.859] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.859] spi-tx: 8f .
[2021-09-29 08:18:25.859] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.859] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.859] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:25.859] spi-tx-rx: 0000 ..
[2021-09-29 08:18:25.859] spi-tx: 0001 ..
[2021-09-29 08:18:25.859] spi-tx: 0001 ..
[2021-09-29 08:18:26.050] spi-tx: 83 .
[2021-09-29 08:18:26.165] spi-tx: 80 .
[2021-09-29 08:18:26.165] spi-tx: 8f .
[2021-09-29 08:18:26.165] spi-tx: 0981 ..
[2021-09-29 08:18:26.165] spi-tx: 0b80 ..
[2021-09-29 08:18:26.165] spi-tx: 1800 ..
[2021-09-29 08:18:26.165] spi-tx: 0002 ..
[2021-09-29 08:18:26.165] spi-tx: 99 .
[2021-09-29 08:18:26.165] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:26.165] spi-tx-rx: 0040 .@
[2021-09-29 08:18:26.165] spi-tx: 83 .
[2021-09-29 08:18:26.165] spi-tx: 80 .
[2021-09-29 08:18:26.165] spi-tx: 8f .
[2021-09-29 08:18:26.165] spi-tx: 0981 ..
[2021-09-29 08:18:26.165] spi-tx: 0b80 ..
[2021-09-29 08:18:26.165] spi-tx: 1800 ..
[2021-09-29 08:18:26.165] spi-tx: 0021 .!
[2021-09-29 08:18:26.165] spi-tx: 010c ..
[2021-09-29 08:18:26.165] spi-tx: 0980 ..
[2021-09-29 08:18:26.165] spi-tx: 1403 ..
[2021-09-29 08:18:26.165] spi-tx: 1800 ..
[2021-09-29 08:18:26.165] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:26.258] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.258] spi-tx-rx: 0080 ..
[2021-09-29 08:18:26.258] spi-tx: 8f .
[2021-09-29 08:18:26.258] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.258] spi-tx-rx: 0040 .@
[2021-09-29 08:18:26.258] RX_COMPLETE
[2021-09-29 08:18:26.258] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:26.258] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.258] spi-tx: 8f .
[2021-09-29 08:18:26.258] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.258] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.258] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.258] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.258] spi-tx: 0001 ..
[2021-09-29 08:18:26.258] spi-tx: 0001 ..
[2021-09-29 08:18:26.449] spi-tx: 83 .
[2021-09-29 08:18:26.563] spi-tx: 80 .
[2021-09-29 08:18:26.563] spi-tx: 8f .
[2021-09-29 08:18:26.563] spi-tx: 0981 ..
[2021-09-29 08:18:26.563] spi-tx: 0b80 ..
[2021-09-29 08:18:26.563] spi-tx: 1800 ..
[2021-09-29 08:18:26.563] spi-tx: 0002 ..
[2021-09-29 08:18:26.563] spi-tx: 99 .
[2021-09-29 08:18:26.563] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:26.563] spi-tx-rx: 0040 .@
[2021-09-29 08:18:26.563] spi-tx: 83 .
[2021-09-29 08:18:26.563] spi-tx: 80 .
[2021-09-29 08:18:26.564] spi-tx: 8f .
[2021-09-29 08:18:26.564] spi-tx: 0981 ..
[2021-09-29 08:18:26.564] spi-tx: 0b80 ..
[2021-09-29 08:18:26.564] spi-tx: 1800 ..
[2021-09-29 08:18:26.564] spi-tx: 0021 .!
[2021-09-29 08:18:26.564] spi-tx: 010c ..
[2021-09-29 08:18:26.564] spi-tx: 0980 ..
[2021-09-29 08:18:26.564] spi-tx: 1403 ..
[2021-09-29 08:18:26.564] spi-tx: 1800 ..
[2021-09-29 08:18:26.564] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:26.658] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.658] spi-tx-rx: 0080 ..
[2021-09-29 08:18:26.658] spi-tx: 8f .
[2021-09-29 08:18:26.658] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.658] spi-tx-rx: 0040 .@
[2021-09-29 08:18:26.658] RX_COMPLETE
[2021-09-29 08:18:26.658] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:26.658] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.658] spi-tx: 8f .
[2021-09-29 08:18:26.658] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.658] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.658] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:26.658] spi-tx-rx: 0000 ..
[2021-09-29 08:18:26.658] spi-tx: 0001 ..
[2021-09-29 08:18:26.658] spi-tx: 0001 ..
[2021-09-29 08:18:26.848] spi-tx: 83 .
[2021-09-29 08:18:26.963] spi-tx: 80 .
[2021-09-29 08:18:26.963] spi-tx: 8f .
[2021-09-29 08:18:26.963] spi-tx: 0981 ..
[2021-09-29 08:18:26.963] spi-tx: 0b80 ..
[2021-09-29 08:18:26.963] spi-tx: 1800 ..
[2021-09-29 08:18:26.963] spi-tx: 0002 ..
[2021-09-29 08:18:26.963] spi-tx: 99 .
[2021-09-29 08:18:26.963] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:26.963] spi-tx-rx: 0040 .@
[2021-09-29 08:18:26.963] spi-tx: 83 .
[2021-09-29 08:18:26.963] spi-tx: 80 .
[2021-09-29 08:18:26.963] spi-tx: 8f .
[2021-09-29 08:18:26.963] spi-tx: 0981 ..
[2021-09-29 08:18:26.963] spi-tx: 0b80 ..
[2021-09-29 08:18:26.963] spi-tx: 1800 ..
[2021-09-29 08:18:26.963] spi-tx: 0021 .!
[2021-09-29 08:18:26.963] spi-tx: 010c ..
[2021-09-29 08:18:26.963] spi-tx: 0980 ..
[2021-09-29 08:18:26.963] spi-tx: 1403 ..
[2021-09-29 08:18:26.963] spi-tx: 1800 ..
[2021-09-29 08:18:26.963] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:27.057] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.057] spi-tx-rx: 0080 ..
[2021-09-29 08:18:27.057] spi-tx: 8f .
[2021-09-29 08:18:27.057] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.057] spi-tx-rx: 0040 .@
[2021-09-29 08:18:27.057] RX_COMPLETE
[2021-09-29 08:18:27.057] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:27.057] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.057] spi-tx: 8f .
[2021-09-29 08:18:27.057] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.057] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.057] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.057] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.057] spi-tx: 0001 ..
[2021-09-29 08:18:27.057] spi-tx: 0001 ..
[2021-09-29 08:18:27.248] spi-tx: 83 .
[2021-09-29 08:18:27.362] spi-tx: 80 .
[2021-09-29 08:18:27.362] spi-tx: 8f .
[2021-09-29 08:18:27.362] spi-tx: 0981 ..
[2021-09-29 08:18:27.362] spi-tx: 0b80 ..
[2021-09-29 08:18:27.362] spi-tx: 1800 ..
[2021-09-29 08:18:27.362] spi-tx: 0002 ..
[2021-09-29 08:18:27.362] spi-tx: 99 .
[2021-09-29 08:18:27.362] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:27.362] spi-tx-rx: 0040 .@
[2021-09-29 08:18:27.362] spi-tx: 83 .
[2021-09-29 08:18:27.362] spi-tx: 80 .
[2021-09-29 08:18:27.362] spi-tx: 8f .
[2021-09-29 08:18:27.362] spi-tx: 0981 ..
[2021-09-29 08:18:27.362] spi-tx: 0b80 ..
[2021-09-29 08:18:27.362] spi-tx: 1800 ..
[2021-09-29 08:18:27.362] spi-tx: 0021 .!
[2021-09-29 08:18:27.362] spi-tx: 010c ..
[2021-09-29 08:18:27.362] spi-tx: 0980 ..
[2021-09-29 08:18:27.362] spi-tx: 1403 ..
[2021-09-29 08:18:27.362] spi-tx: 1800 ..
[2021-09-29 08:18:27.362] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:27.457] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.457] spi-tx-rx: 0080 ..
[2021-09-29 08:18:27.457] spi-tx: 8f .
[2021-09-29 08:18:27.457] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.457] spi-tx-rx: 0040 .@
[2021-09-29 08:18:27.457] RX_COMPLETE
[2021-09-29 08:18:27.457] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:27.457] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.457] spi-tx: 8f .
[2021-09-29 08:18:27.457] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.457] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.457] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.457] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.457] spi-tx: 0001 ..
[2021-09-29 08:18:27.457] spi-tx: 0001 ..
[2021-09-29 08:18:27.646] spi-tx: 83 .
[2021-09-29 08:18:27.762] spi-tx: 80 .
[2021-09-29 08:18:27.762] spi-tx: 8f .
[2021-09-29 08:18:27.762] spi-tx: 0981 ..
[2021-09-29 08:18:27.762] spi-tx: 0b80 ..
[2021-09-29 08:18:27.762] spi-tx: 1800 ..
[2021-09-29 08:18:27.762] spi-tx: 0002 ..
[2021-09-29 08:18:27.762] spi-tx: 99 .
[2021-09-29 08:18:27.762] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:27.762] spi-tx-rx: 0040 .@
[2021-09-29 08:18:27.762] spi-tx: 83 .
[2021-09-29 08:18:27.762] spi-tx: 80 .
[2021-09-29 08:18:27.762] spi-tx: 8f .
[2021-09-29 08:18:27.762] spi-tx: 0981 ..
[2021-09-29 08:18:27.762] spi-tx: 0b80 ..
[2021-09-29 08:18:27.762] spi-tx: 1800 ..
[2021-09-29 08:18:27.762] spi-tx: 0021 .!
[2021-09-29 08:18:27.762] spi-tx: 010c ..
[2021-09-29 08:18:27.762] spi-tx: 0980 ..
[2021-09-29 08:18:27.762] spi-tx: 1403 ..
[2021-09-29 08:18:27.762] spi-tx: 1800 ..
[2021-09-29 08:18:27.762] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:27.855] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.855] spi-tx-rx: 0080 ..
[2021-09-29 08:18:27.855] spi-tx: 8f .
[2021-09-29 08:18:27.855] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.855] spi-tx-rx: 0040 .@
[2021-09-29 08:18:27.855] RX_COMPLETE
[2021-09-29 08:18:27.855] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:27.855] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.855] spi-tx: 8f .
[2021-09-29 08:18:27.855] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.855] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.855] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:27.855] spi-tx-rx: 0000 ..
[2021-09-29 08:18:27.855] spi-tx: 0001 ..
[2021-09-29 08:18:27.855] spi-tx: 0001 ..
[2021-09-29 08:18:28.047] spi-tx: 83 .
[2021-09-29 08:18:28.161] spi-tx: 80 .
[2021-09-29 08:18:28.161] spi-tx: 8f .
[2021-09-29 08:18:28.161] spi-tx: 0981 ..
[2021-09-29 08:18:28.161] spi-tx: 0b80 ..
[2021-09-29 08:18:28.161] spi-tx: 1800 ..
[2021-09-29 08:18:28.161] spi-tx: 0002 ..
[2021-09-29 08:18:28.161] spi-tx: 99 .
[2021-09-29 08:18:28.161] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:28.161] spi-tx-rx: 0040 .@
[2021-09-29 08:18:28.161] spi-tx: 83 .
[2021-09-29 08:18:28.161] spi-tx: 80 .
[2021-09-29 08:18:28.161] spi-tx: 8f .
[2021-09-29 08:18:28.161] spi-tx: 0981 ..
[2021-09-29 08:18:28.161] spi-tx: 0b80 ..
[2021-09-29 08:18:28.161] spi-tx: 1800 ..
[2021-09-29 08:18:28.161] spi-tx: 0021 .!
[2021-09-29 08:18:28.161] spi-tx: 010c ..
[2021-09-29 08:18:28.161] spi-tx: 0980 ..
[2021-09-29 08:18:28.161] spi-tx: 1403 ..
[2021-09-29 08:18:28.161] spi-tx: 1800 ..
[2021-09-29 08:18:28.161] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:28.255] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.255] spi-tx-rx: 0080 ..
[2021-09-29 08:18:28.255] spi-tx: 8f .
[2021-09-29 08:18:28.255] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.255] spi-tx-rx: 0040 .@
[2021-09-29 08:18:28.255] RX_COMPLETE
[2021-09-29 08:18:28.255] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:28.255] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.255] spi-tx: 8f .
[2021-09-29 08:18:28.255] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.255] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.255] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.255] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.255] spi-tx: 0001 ..
[2021-09-29 08:18:28.255] spi-tx: 0001 ..
[2021-09-29 08:18:28.445] spi-tx: 83 .
[2021-09-29 08:18:28.560] spi-tx: 80 .
[2021-09-29 08:18:28.560] spi-tx: 8f .
[2021-09-29 08:18:28.560] spi-tx: 0981 ..
[2021-09-29 08:18:28.560] spi-tx: 0b80 ..
[2021-09-29 08:18:28.560] spi-tx: 1800 ..
[2021-09-29 08:18:28.560] spi-tx: 0002 ..
[2021-09-29 08:18:28.560] spi-tx: 99 .
[2021-09-29 08:18:28.560] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:28.560] spi-tx-rx: 0040 .@
[2021-09-29 08:18:28.560] spi-tx: 83 .
[2021-09-29 08:18:28.560] spi-tx: 80 .
[2021-09-29 08:18:28.560] spi-tx: 8f .
[2021-09-29 08:18:28.560] spi-tx: 0981 ..
[2021-09-29 08:18:28.560] spi-tx: 0b80 ..
[2021-09-29 08:18:28.561] spi-tx: 1800 ..
[2021-09-29 08:18:28.561] spi-tx: 0021 .!
[2021-09-29 08:18:28.561] spi-tx: 010c ..
[2021-09-29 08:18:28.561] spi-tx: 0980 ..
[2021-09-29 08:18:28.561] spi-tx: 1403 ..
[2021-09-29 08:18:28.561] spi-tx: 1800 ..
[2021-09-29 08:18:28.561] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:28.654] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.654] spi-tx-rx: 0080 ..
[2021-09-29 08:18:28.654] spi-tx: 8f .
[2021-09-29 08:18:28.654] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.654] spi-tx-rx: 0040 .@
[2021-09-29 08:18:28.654] RX_COMPLETE
[2021-09-29 08:18:28.654] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:28.654] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.654] spi-tx: 8f .
[2021-09-29 08:18:28.654] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.654] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.654] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:28.654] spi-tx-rx: 0000 ..
[2021-09-29 08:18:28.654] spi-tx: 0001 ..
[2021-09-29 08:18:28.654] spi-tx: 0001 ..
[2021-09-29 08:18:28.845] spi-tx: 83 .
[2021-09-29 08:18:28.960] spi-tx: 80 .
[2021-09-29 08:18:28.960] spi-tx: 8f .
[2021-09-29 08:18:28.960] spi-tx: 0981 ..
[2021-09-29 08:18:28.960] spi-tx: 0b80 ..
[2021-09-29 08:18:28.960] spi-tx: 1800 ..
[2021-09-29 08:18:28.960] spi-tx: 0002 ..
[2021-09-29 08:18:28.960] spi-tx: 99 .
[2021-09-29 08:18:28.960] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:28.960] spi-tx-rx: 0040 .@
[2021-09-29 08:18:28.960] spi-tx: 83 .
[2021-09-29 08:18:28.960] spi-tx: 80 .
[2021-09-29 08:18:28.960] spi-tx: 8f .
[2021-09-29 08:18:28.960] spi-tx: 0981 ..
[2021-09-29 08:18:28.960] spi-tx: 0b80 ..
[2021-09-29 08:18:28.960] spi-tx: 1800 ..
[2021-09-29 08:18:28.960] spi-tx: 0021 .!
[2021-09-29 08:18:28.960] spi-tx: 010c ..
[2021-09-29 08:18:28.960] spi-tx: 0980 ..
[2021-09-29 08:18:28.960] spi-tx: 1403 ..
[2021-09-29 08:18:28.960] spi-tx: 1800 ..
[2021-09-29 08:18:28.960] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:29.053] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.053] spi-tx-rx: 0080 ..
[2021-09-29 08:18:29.053] spi-tx: 8f .
[2021-09-29 08:18:29.053] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.053] spi-tx-rx: 0040 .@
[2021-09-29 08:18:29.053] RX_COMPLETE
[2021-09-29 08:18:29.053] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:29.053] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.053] spi-tx: 8f .
[2021-09-29 08:18:29.053] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.053] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.053] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.053] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.053] spi-tx: 0001 ..
[2021-09-29 08:18:29.053] spi-tx: 0001 ..
[2021-09-29 08:18:29.244] spi-tx: 83 .
[2021-09-29 08:18:29.359] spi-tx: 80 .
[2021-09-29 08:18:29.359] spi-tx: 8f .
[2021-09-29 08:18:29.359] spi-tx: 0981 ..
[2021-09-29 08:18:29.359] spi-tx: 0b80 ..
[2021-09-29 08:18:29.359] spi-tx: 1800 ..
[2021-09-29 08:18:29.359] spi-tx: 0002 ..
[2021-09-29 08:18:29.359] spi-tx: 99 .
[2021-09-29 08:18:29.359] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:29.359] spi-tx-rx: 0040 .@
[2021-09-29 08:18:29.359] spi-tx: 83 .
[2021-09-29 08:18:29.359] spi-tx: 80 .
[2021-09-29 08:18:29.359] spi-tx: 8f .
[2021-09-29 08:18:29.359] spi-tx: 0981 ..
[2021-09-29 08:18:29.359] spi-tx: 0b80 ..
[2021-09-29 08:18:29.359] spi-tx: 1800 ..
[2021-09-29 08:18:29.359] spi-tx: 0021 .!
[2021-09-29 08:18:29.359] spi-tx: 010c ..
[2021-09-29 08:18:29.359] spi-tx: 0980 ..
[2021-09-29 08:18:29.359] spi-tx: 1403 ..
[2021-09-29 08:18:29.359] spi-tx: 1800 ..
[2021-09-29 08:18:29.359] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:29.453] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.453] spi-tx-rx: 0080 ..
[2021-09-29 08:18:29.453] spi-tx: 8f .
[2021-09-29 08:18:29.453] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.453] spi-tx-rx: 0040 .@
[2021-09-29 08:18:29.453] RX_COMPLETE
[2021-09-29 08:18:29.453] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:29.453] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.453] spi-tx: 8f .
[2021-09-29 08:18:29.453] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.453] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.453] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.453] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.453] spi-tx: 0001 ..
[2021-09-29 08:18:29.453] spi-tx: 0001 ..
[2021-09-29 08:18:29.644] spi-tx: 83 .
[2021-09-29 08:18:29.752] spi-tx: 80 .
[2021-09-29 08:18:29.752] spi-tx: 8f .
[2021-09-29 08:18:29.752] spi-tx: 0981 ..
[2021-09-29 08:18:29.752] spi-tx: 0b80 ..
[2021-09-29 08:18:29.752] spi-tx: 1800 ..
[2021-09-29 08:18:29.752] spi-tx: 0002 ..
[2021-09-29 08:18:29.752] spi-tx: 99 .
[2021-09-29 08:18:29.752] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:29.752] spi-tx-rx: 0040 .@
[2021-09-29 08:18:29.752] spi-tx: 83 .
[2021-09-29 08:18:29.752] spi-tx: 80 .
[2021-09-29 08:18:29.752] spi-tx: 8f .
[2021-09-29 08:18:29.752] spi-tx: 0981 ..
[2021-09-29 08:18:29.752] spi-tx: 0b80 ..
[2021-09-29 08:18:29.752] spi-tx: 1800 ..
[2021-09-29 08:18:29.752] spi-tx: 0021 .!
[2021-09-29 08:18:29.752] spi-tx: 010c ..
[2021-09-29 08:18:29.752] spi-tx: 0980 ..
[2021-09-29 08:18:29.752] spi-tx: 1403 ..
[2021-09-29 08:18:29.752] spi-tx: 1800 ..
[2021-09-29 08:18:29.852] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:29.852] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.852] spi-tx-rx: 0080 ..
[2021-09-29 08:18:29.852] spi-tx: 8f .
[2021-09-29 08:18:29.852] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.852] spi-tx-rx: 0040 .@
[2021-09-29 08:18:29.852] RX_COMPLETE
[2021-09-29 08:18:29.852] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:29.852] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.852] spi-tx: 8f .
[2021-09-29 08:18:29.852] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.852] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.852] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:29.852] spi-tx-rx: 0000 ..
[2021-09-29 08:18:29.852] spi-tx: 0001 ..
[2021-09-29 08:18:29.852] spi-tx: 0001 ..
[2021-09-29 08:18:30.043] spi-tx: 83 .
[2021-09-29 08:18:30.151] spi-tx: 80 .
[2021-09-29 08:18:30.151] spi-tx: 8f .
[2021-09-29 08:18:30.151] spi-tx: 0981 ..
[2021-09-29 08:18:30.151] spi-tx: 0b80 ..
[2021-09-29 08:18:30.151] spi-tx: 1800 ..
[2021-09-29 08:18:30.151] spi-tx: 0002 ..
[2021-09-29 08:18:30.151] spi-tx: 99 .
[2021-09-29 08:18:30.151] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:30.151] spi-tx-rx: 0040 .@
[2021-09-29 08:18:30.151] spi-tx: 83 .
[2021-09-29 08:18:30.151] spi-tx: 80 .
[2021-09-29 08:18:30.151] spi-tx: 8f .
[2021-09-29 08:18:30.151] spi-tx: 0981 ..
[2021-09-29 08:18:30.151] spi-tx: 0b80 ..
[2021-09-29 08:18:30.151] spi-tx: 1800 ..
[2021-09-29 08:18:30.151] spi-tx: 0021 .!
[2021-09-29 08:18:30.151] spi-tx: 010c ..
[2021-09-29 08:18:30.151] spi-tx: 0980 ..
[2021-09-29 08:18:30.151] spi-tx: 1403 ..
[2021-09-29 08:18:30.151] spi-tx: 1800 ..
[2021-09-29 08:18:30.251] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:30.251] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.251] spi-tx-rx: 0080 ..
[2021-09-29 08:18:30.251] spi-tx: 8f .
[2021-09-29 08:18:30.251] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.251] spi-tx-rx: 0040 .@
[2021-09-29 08:18:30.251] RX_COMPLETE
[2021-09-29 08:18:30.251] spi-tx-tx: 5c00 \.
[2021-09-29 08:18:30.251] spi-tx-rx: 0000 ..
[2021-09-29 08:18:30.251] spi-tx: 8f .
[2021-09-29 08:18:30.251] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.251] spi-tx-rx: 0000 ..
[2021-09-29 08:18:30.251] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.251] spi-tx-rx: 0000 ..
[2021-09-29 08:18:30.251] spi-tx: 0001 ..
[2021-09-29 08:18:30.251] spi-tx: 0001 ..
[2021-09-29 08:18:30.442] spi-tx: 83 .
[2021-09-29 08:18:30.550] spi-tx: 80 .
[2021-09-29 08:18:30.550] spi-tx: 8f .
[2021-09-29 08:18:30.550] spi-tx: 0981 ..
[2021-09-29 08:18:30.550] spi-tx: 0b80 ..
[2021-09-29 08:18:30.550] spi-tx: 1800 ..
[2021-09-29 08:18:30.550] spi-tx: 0002 ..
[2021-09-29 08:18:30.550] spi-tx: 99 .
[2021-09-29 08:18:30.550] spi-tx-tx: 4f00 O.
[2021-09-29 08:18:30.550] spi-tx-rx: 0040 .@
[2021-09-29 08:18:30.550] spi-tx: 83 .
[2021-09-29 08:18:30.550] spi-tx: 80 .
[2021-09-29 08:18:30.550] spi-tx: 8f .
[2021-09-29 08:18:30.550] spi-tx: 0981 ..
[2021-09-29 08:18:30.550] spi-tx: 0b80 ..
[2021-09-29 08:18:30.550] spi-tx: 1800 ..
[2021-09-29 08:18:30.550] spi-tx: 0021 .!
[2021-09-29 08:18:30.550] spi-tx: 010c ..
[2021-09-29 08:18:30.550] spi-tx: 0980 ..
[2021-09-29 08:18:30.550] spi-tx: 1403 ..
[2021-09-29 08:18:30.550] spi-tx: 1800 ..
[2021-09-29 08:18:30.596] spi-tx: 8f913d0030050000 ..=.0...
[2021-09-29 08:18:30.596] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.596] spi-tx-rx: 0080 ..
[2021-09-29 08:18:30.596] spi-tx: 8f .
[2021-09-29 08:18:30.596] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.596] spi-tx-rx: 0000 ..
[2021-09-29 08:18:30.652] spi-tx-tx: 4c00 L.
[2021-09-29 08:18:30.652] spi-tx-rx: 0000 ..
[2021-09-29 08:18:30.652] spi-tx: 0001 ..
[2021-09-29 08:18:30.652] spi-tx: 0001 ..