Other Parts Discussed in Thread: TRF7970A, TRF7964A
Hi,
My customer is developing the system using TRF7960A.
As TRF7960AEVM is no longer available, customer uses TRF7970A for development.
Customer refers below FAQ document.
https://www.tij.co.jp/jp/lit/an/sloa248b/sloa248b.pdf
Now they are able to send/receive all necessary ICODE commands with TRF7970A.
But some commands fails when the device is replaced with TRF7960A which will be used for their production.
ICODE used is NXP SL2S2602 (ICODE SLIX2).
https://www.nxp.com/docs/en/data-sheet/SL2S2602.pdf
An example of failing commands is Set Password.
Set Password command is 16bytes, but TRF7960A has only 12bytes FIFO. So customer sent 12bytes + 4bytes=16bytes.
Here are SPI waveforms between MCU and TRF7960A.
SLIX2_setPassword: Start of the command to the end of the command.
There are 5bytes header at the beginning of SPI data, so total 17 bytes(5+12bytes) are sent at the first half. 
SLIX2_setPassword(zoom): Zoom up of the later half of the command.
At the 1st circle, IRQ is generated and IRQ register(0x0C) is 0x80. This is irq_tx.
Then 2nd circle is remaining 4 bytes with leading byte(0x3F), so total 5 bytes.
As you can see, just before the 2nd circle, another IRQ is generated and IRQ register is read at the 3rd circle.
The register value is 0x40. This is Irq_srx.
The code is based on TI example (trf79xxxa.c).
The Irq_srx happens while the code is running line#505 (while loop) and TRF79xxA_irqHandler() is called.
Then g_sTrfStatus="RX_COMPLETE" is returned and it results in g_sTrfStatus="TX_ERROR".
/*
* File Name: trf797x.c
*
* Description: TRF797x Driver Functions
*
* Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
#include "trf79xxa.h"
//===============================================================
uint8_t g_pui8TrfBuffer[NFC_FIFO_SIZE];
static uint8_t g_ui8CollisionPosition;
static uint8_t g_ui8FifoOffset;
static uint8_t g_ui8FifoRxLength;
static tTrfStatus g_sTrfStatus;
static tTrfSettings g_eTrfGeneralSettings;
static volatile uint8_t g_ui8IrqFlag;
static volatile uint8_t g_ui8TimeoutFlag;
//*****************************************************************************
//
//! \addtogroup trf797x_api TRF7970A Driver API's
//! @{
//!
//! This section describes all the functions contained within the TRF79xxA
//! driver.
//
//*****************************************************************************
//===============================================================
//
//! TRF79xxA_sendDirectCommand - Send a Direct Command to TRF79xxA.
//!
//! \param ui8Value is the direct command to be issued
//!
//! This function is used to transmit a Direct Command to TRF79xxA.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_sendDirectCommand(uint8_t ui8Value)
{
SPI_directCommand(ui8Value);
}
//===============================================================
//
//! TRF79xxA_disableSlotCounter - Disables interrupts from 15693
//! slot counter function.
//!
//! This function will configure the TRF79xxA to disable the
//! firing of the IRQ interrupt when an ISO15693 slot marker
//! hits the No Response timeout threshold.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_disableSlotCounter(void)
{
uint8_t ui8Value;
ui8Value = TRF79xxA_readRegister(TRF79XXA_IRQ_MASK);
ui8Value &= 0xFE; // Clear BIT0 in register 0x0D
TRF79xxA_writeRegister(TRF79XXA_IRQ_MASK,ui8Value);
}
//===============================================================
//
//! TRF79xxA_enableSlotCounter - Enables interrupts from 15693
//! slot counter function.
//!
//! This function will configure the TRF79xxA to enable the
//! firing of the IRQ interrupt when an ISO15693 slot marker
//! hits the No Response timeout threshold.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_enableSlotCounter(void)
{
uint8_t ui8Value;
ui8Value = TRF79xxA_readRegister(TRF79XXA_IRQ_MASK);
ui8Value |= BIT0; // Set BIT0 in register 0x0D
TRF79xxA_writeRegister(TRF79XXA_IRQ_MASK,ui8Value);
}
//===============================================================
//
//! TRF79xxA_resetFIFO - Resets TRF79xxA FIFO
//!
//! This function used to reset the TRF79xxA FIFO.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_resetFIFO(void)
{
uint8_t ui8Command;
ui8Command = TRF79XXA_RESET_FIFO_CMD;
TRF79xxA_sendDirectCommand(ui8Command);
}
//===============================================================
//
//! TRF79xxA_initialSettings - Initialize TRF79xxA
//!
//! This function configures the TRF79xxA upon power up.
//! Steps include:
//! - Setup SPI communication
//! - Send Soft Init and Idle Direct Commands
//! - Reset the FIFO
//! - Configure TRF79xxA modulator and regulator registers
//! - TRF7970A only: Write to regiser 0x18 per errata
//!
//! \return None.
//
//===============================================================
void TRF79xxA_initialSettings(void)
{
g_ui8CollisionPosition = 0;
g_ui8FifoOffset = 0;
g_ui8FifoRxLength = 0;
g_sTrfStatus = TRF_IDLE;
g_eTrfGeneralSettings.eTrfPowerSetting = TRF79xxA_3V_FULL_POWER;
g_eTrfGeneralSettings.bRfFieldOn = false;
g_eTrfGeneralSettings.ui8IsoControl = 0x02; // TRF79xxA Default
g_ui8IrqFlag = 0x00;
g_ui8TimeoutFlag = 0x00;
// Setup TRF79xxA SPI Module
SPI_setup();
// Delay to allow SPI to finish starting up
MCU_delayMillisecond(1);
// Send out SOFT_INIT + IDLE initial sequence to soft reset TRF7970A
TRF79xxA_sendDirectCommand(TRF79XXA_SOFT_INIT_CMD);
TRF79xxA_sendDirectCommand(TRF79XXA_IDLE_CMD);
// Delay to ensure soft reset has processed
MCU_delayMillisecond(1);
#if (TRF79xxA_VERSION == 70)
g_eTrfGeneralSettings.ui8IsoControl = 0x21;
#elif (TRF79xxA_VERSION == 60)
g_eTrfGeneralSettings.ui8IsoControl = 0x02;
#endif
TRF79xxA_resetFIFO(); // Reset the FIFO
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x01); // ASK 100%, no SYS_CLK output
TRF79xxA_writeRegister(TRF79XXA_REGULATOR_CONTROL, 0x01);
#if (TRF79xxA_VERSION == 70)
TRF79xxA_writeRegister(TRF79XXA_NFC_TARGET_LEVEL, 0x00); // For TRF7970A Errata
#endif
}
//===============================================================
//
//! TRF79xxA_processIRQ - Services TRF79xxA IRQ interrupts
//!
//! \param pui8IrqStatus is the received IRQ Status flags
//!
//! The Interrupt Service Routine determines how the IRQ should
//! be handled. The TRF79xxA IRQ status register is read to
//! determine the cause of the IRQ. Conditions are checked and
//! appropriate actions taken.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_processIRQ(uint8_t * pui8IrqStatus)
{
uint8_t ui8DummyRead;
uint8_t ui8Length;
if(*pui8IrqStatus == (TRF79XXA_IRQ_STATUS_TX_COMPLETE | TRF79XXA_IRQ_STATUS_FIFO_HIGH_OR_LOW)) // BIT5 and BIT7
{ // TX active and 32 bytes left in FIFO
g_sTrfStatus = TX_COMPLETE;
}
else if(*pui8IrqStatus == TRF79XXA_IRQ_STATUS_TX_COMPLETE)
{ // TX complete
g_sTrfStatus = TX_COMPLETE;
TRF79xxA_resetFIFO(); // reset the FIFO after TX
}
else if((*pui8IrqStatus & BIT1) == TRF79XXA_IRQ_STATUS_COLLISION_ERROR)
{ // Collision error
if ((g_eTrfGeneralSettings.ui8IsoControl == 0x08) || (g_eTrfGeneralSettings.ui8IsoControl == 0x88))
{
g_sTrfStatus = COLLISION_ERROR;
g_ui8CollisionPosition = TRF79xxA_readRegister(TRF79XXA_COLLISION_POSITION);
if (g_ui8CollisionPosition > 0x20)
{
ui8Length = g_ui8CollisionPosition - 0x20; // number of valid bytes in FIFO
if((ui8Length & 0x0F) != 0x00)
{
ui8Length = ui8Length + 0x10; // add 1 byte if broken byte recieved
}
ui8Length = ui8Length >> 4;
if(ui8Length != 0x00)
{
g_pui8TrfBuffer[g_ui8FifoOffset] = TRF79XXA_FIFO; // write the recieved bytes to the correct place of the buffer
TRF79xxA_readContinuous(&g_pui8TrfBuffer[g_ui8FifoOffset], ui8Length);
g_ui8FifoOffset = g_ui8FifoOffset + ui8Length;
}
}
else
{
g_ui8FifoRxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
#if (TRF79xxA_VERSION == 70)
g_ui8FifoRxLength &= 0x7F;
#elif (TRF79xxA_VERSION == 60)
g_ui8FifoRxLength = (0x0F & g_ui8FifoRxLength) + 1;
#endif
g_pui8TrfBuffer[g_ui8FifoOffset] = TRF79XXA_FIFO; // write the recieved bytes to the correct place of the buffer
TRF79xxA_readContinuous(&g_pui8TrfBuffer[g_ui8FifoOffset], g_ui8FifoRxLength);
g_ui8FifoOffset = g_ui8FifoOffset + g_ui8FifoRxLength;
}
}
else if((g_eTrfGeneralSettings.ui8IsoControl & 0xF8) == 0x00) // Covers all ISO15693 Data Rates for RFID mode with RX CRC on
{
g_sTrfStatus = COLLISION_ERROR;
}
else
{
g_sTrfStatus = PROTOCOL_ERROR;
}
TRF79xxA_sendDirectCommand(TRF79XXA_STOP_DECODERS_CMD);
TRF79xxA_resetFIFO(); // reset the FIFO after TX
TRF79xxA_resetIrqStatus();
IRQ_CLR;
}
else if(*pui8IrqStatus == TRF79XXA_IRQ_STATUS_RX_COMPLETE)
{ // RX flag means that EOF has been recieved
// and the number of unread bytes is in FIFOstatus regiter
g_ui8FifoRxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
#if (TRF79xxA_VERSION == 70)
g_ui8FifoRxLength &= 0x7F;
#elif (TRF79xxA_VERSION == 60)
g_ui8FifoRxLength = (0x0F & g_ui8FifoRxLength) + 1;
#endif
g_pui8TrfBuffer[g_ui8FifoOffset] = TRF79XXA_FIFO; // write the received bytes to the correct place of the buffer
TRF79xxA_readContinuous(&g_pui8TrfBuffer[g_ui8FifoOffset], g_ui8FifoRxLength);
g_ui8FifoOffset = g_ui8FifoOffset + g_ui8FifoRxLength;
TRF79xxA_resetFIFO(); // reset the FIFO after last byte has been read out
if (g_sTrfStatus == RX_WAIT_EXTENSION)
{
g_ui8FifoRxLength = g_ui8FifoOffset;
}
g_sTrfStatus = RX_COMPLETE;
}
else if(*pui8IrqStatus == (TRF79XXA_IRQ_STATUS_RX_COMPLETE | TRF79XXA_IRQ_STATUS_FIFO_HIGH_OR_LOW))
{ // RX active and 96 bytes allready in FIFO
g_sTrfStatus = RX_WAIT;
// Read FIFO Status to determine how many bytes are in the FIFO
g_ui8FifoRxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
#if (TRF79xxA_VERSION == 70)
g_ui8FifoRxLength &= 0x7F;
#elif (TRF79xxA_VERSION == 60)
g_ui8FifoRxLength = (0x0F & g_ui8FifoRxLength) + 1;
#endif
if (NFC_FIFO_SIZE > (g_ui8FifoOffset+g_ui8FifoRxLength))
{
// Read from the FIFO to empty it
g_pui8TrfBuffer[g_ui8FifoOffset] = TRF79XXA_FIFO;
TRF79xxA_readContinuous(&g_pui8TrfBuffer[g_ui8FifoOffset], g_ui8FifoRxLength); // read all received bytes from FIFO
g_ui8FifoOffset = g_ui8FifoOffset + g_ui8FifoRxLength; // Adjust buffer index
}
else
{
g_sTrfStatus = PROTOCOL_ERROR;
return;
}
#if (TRF79xxA_VERSION == 70)
// Read FIFO Status again to determine if more bytes have been received
g_ui8FifoRxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
g_ui8FifoRxLength &= 0x7F;
if (g_ui8FifoRxLength > 0)
{
g_sTrfStatus = RX_WAIT_EXTENSION;
}
else
{
g_ui8FifoRxLength = g_ui8FifoOffset;
g_sTrfStatus = RX_COMPLETE;
return;
}
#elif (TRF79xxA_VERSION == 60)
// Cannot rely on FIFO Status results to indicate number of bytes left, therefore always must go to RX_WAIT_EXTENSION state.
g_sTrfStatus = RX_WAIT_EXTENSION;
g_ui8FifoRxLength = g_ui8FifoOffset;
#endif
}
else if (*pui8IrqStatus == (TRF79XXA_IRQ_STATUS_RX_COMPLETE | TRF79XXA_IRQ_STATUS_NO_RESPONSE))
{
// RX has begun but as not completed, space exists in FIFO still, just wait longer to receive full reply.
g_sTrfStatus = RX_WAIT_EXTENSION;
}
else if((*pui8IrqStatus & BIT4) == TRF79XXA_IRQ_STATUS_CRC_ERROR) // CRC error
{
if((*pui8IrqStatus & BIT6) == TRF79XXA_IRQ_STATUS_RX_COMPLETE) // 4 Bit receive
{
ui8DummyRead = TRF79XXA_FIFO; // write the recieved bytes to the correct place of the buffer
TRF79xxA_readContinuous(&ui8DummyRead, 1);
}
TRF79xxA_reset();
g_sTrfStatus = PROTOCOL_ERROR;
}
else if((*pui8IrqStatus & BIT2) == TRF79XXA_IRQ_STATUS_FRAMING_ERROR) // byte framing error
{
if((*pui8IrqStatus & BIT5) == TRF79XXA_IRQ_STATUS_FIFO_HIGH_OR_LOW)
{
g_sTrfStatus = RX_WAIT;
}
else if ((*pui8IrqStatus & BIT6) == TRF79XXA_IRQ_STATUS_RX_COMPLETE)
{
if((g_eTrfGeneralSettings.ui8IsoControl & 0xF8) == 0x00) // Covers all ISO15693 Data Rates for RFID mode with RX CRC on
{
g_sTrfStatus = COLLISION_ERROR;
}
else
{
g_sTrfStatus = PROTOCOL_ERROR;
TRF79xxA_reset();
}
}
else
{
g_sTrfStatus = PROTOCOL_ERROR;
TRF79xxA_reset();
}
}
else if(*pui8IrqStatus == TRF79XXA_IRQ_STATUS_IDLE)
{ // No response interrupt
g_sTrfStatus = NO_RESPONSE_RECEIVED;
}
else if(*pui8IrqStatus == TRF79XXA_IRQ_STATUS_NO_RESPONSE)
{ // No response interrupt
g_sTrfStatus = NO_RESPONSE_RECEIVED_15693;
g_ui8FifoOffset = 0;
}
else
{ // Interrupt register not properly set
g_sTrfStatus = PROTOCOL_ERROR;
TRF79xxA_sendDirectCommand(TRF79XXA_STOP_DECODERS_CMD); // reset the FIFO after TX
TRF79xxA_reset();
TRF79xxA_resetIrqStatus();
IRQ_CLR;
}
} // Interrupt Service Routine
//===============================================================
//
//! TRF79xxA_writeRaw - Write data to TRF79xxA
//!
//! \param pui8Payload is the buffer with data packet contents
//! \param ui8Length is the size of the data packet
//!
//! This function writes provided data directly to the TRF79xxA.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_writeRaw(uint8_t * pui8Payload, uint8_t ui8Length)
{
uint8_t ui8TxBytesRemaining;
uint8_t ui8TxIndex;
uint8_t ui8FifoTxLength;
uint8_t ui8TxBytesAvailable;
bool bContinuedSend = false;
g_sTrfStatus = TRF_IDLE;
// First send includes 5 bytes for command overhead
if (TRF79xxA_MAX_FIFO_SIZE+5 > ui8Length)
{
SPI_rawWrite(pui8Payload, ui8Length, bContinuedSend);
}
else
{
ui8TxBytesRemaining = ui8Length;
ui8TxIndex = 0;
ui8TxBytesAvailable = TRF79xxA_MAX_FIFO_SIZE+5; // First send includes 5 bytes for command overhead
// (Reset FIFO, Transmit with or without CRC, Continuous Write, Length High and Length Low)
bContinuedSend = false; // First send is not continued
while(ui8TxBytesRemaining > 0)
{
if (ui8TxBytesRemaining > TRF79xxA_MAX_FIFO_SIZE)
{
#if TRF79xxA_VERSION == 60
// Avoid 60A single byte FIFO TX case from sloa140 Section 1.5
if ((ui8TxBytesRemaining - ui8TxBytesAvailable) == 1)
{
SPI_rawWrite(&pui8Payload[ui8TxIndex], ui8TxBytesAvailable-1, bContinuedSend);
ui8TxBytesRemaining = ui8TxBytesRemaining - ui8TxBytesAvailable - 1;
}
else
{
#endif
SPI_rawWrite(&pui8Payload[ui8TxIndex], ui8TxBytesAvailable, bContinuedSend);
ui8TxBytesRemaining = ui8TxBytesRemaining - ui8TxBytesAvailable;
#if TRF79xxA_VERSION == 60
}
#endif
ui8TxIndex = ui8TxIndex + ui8TxBytesAvailable;
bContinuedSend = true;
}
else
{
// Last send
SPI_rawWrite(&pui8Payload[ui8TxIndex], ui8TxBytesRemaining, bContinuedSend);
bContinuedSend = false;
ui8TxBytesRemaining = 0;
}
g_ui8TimeoutFlag = 0x00;
// Clear the IRQ Flag
g_ui8IrqFlag = 0x00;
// Setup for the Timer
MCU_setCounter(5);
while((g_ui8IrqFlag == 0x00) && (g_ui8TimeoutFlag == 0x00)) // Wait for an interrupt
{
// Do Nothing
}
RESET_COUNTER;
if (g_sTrfStatus == TX_WAIT)
{
ui8FifoTxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
#if (TRF79xxA_VERSION == 70)
ui8FifoTxLength &= 0x7F;
#elif (TRF79xxA_VERSION == 60)
ui8FifoTxLength = 0x0F & ui8FifoTxLength;
#endif
ui8TxBytesAvailable = TRF79xxA_MAX_FIFO_SIZE-ui8FifoTxLength;
}
else if (g_sTrfStatus == TX_COMPLETE)
{
if (ui8TxBytesRemaining == 0)
{
// Packet is sent
break;
}
else
{
ui8FifoTxLength = TRF79xxA_readRegister(TRF79XXA_FIFO_STATUS);
#if (TRF79xxA_VERSION == 70)
ui8FifoTxLength &= 0x7F;
#elif (TRF79xxA_VERSION == 60)
ui8FifoTxLength = 0x0F & ui8FifoTxLength;
#endif
ui8TxBytesAvailable = TRF79xxA_MAX_FIFO_SIZE-ui8FifoTxLength;
bContinuedSend = true;
}
}
else
{
// Error occurred, break
g_sTrfStatus = TX_ERROR;
break;
}
}
}
}
//===============================================================
//
//! TRF79xxA_readContinuous - Read multiple TRF79xxA registers
//!
//! \param pui8Payload is the address of the first register as
//! well as the pointer for buffer where the results will be
//! \param ui8Length is the number of registers to read
//!
//! This function reads a specified number of TRF79xxA registers
//! from a specified address.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_readContinuous(uint8_t * pui8Payload, uint8_t ui8Length)
{
SPI_readCont(pui8Payload, ui8Length);
}
//===============================================================
//
//! TRF79xxA_readIrqStatus - Read out the IRQ Status Register
//!
//! This function reads the IRQ Status register of the TRF79xxA
//! and store the result into the location pointed to by the
//! input.
//!
//! \return pui8Value returns the value of the IRQ Status
//! Register
//
//===============================================================
uint8_t TRF79xxA_readIrqStatus(void)
{
uint8_t pui8Value[2];
pui8Value[0] = TRF79XXA_IRQ_STATUS;
#if (TRF79xxA_VERSION == 70)
SPI_readSingle(pui8Value);
#elif (TRF79xxA_VERSION == 60)
SPI_readCont(pui8Value,2); // Dummy read to properly clear IRQ Status for TRF796xA devices (except 64A)
#endif
return pui8Value[0];
}
//===============================================================
//
//! TRF79xxA_readRegister - Read out a single TRF79xxA register
//!
//! This function reads a specific TRF79xxA register.
//!
//! \return pui8Value returns the value of the TRF79xxA Register
//
//===============================================================
uint8_t TRF79xxA_readRegister(uint8_t ui8TrfRegister)
{
uint8_t pui8Value[1];
pui8Value[0] = ui8TrfRegister;
SPI_readSingle(pui8Value);
return pui8Value[0];
}
//===============================================================
//
//! TRF79xxA_reset - Resets TRF79xxA
//!
//! This function will reset the TRF79xxA through the Software
//! Init direct command followed by reinitializing basic settings
//! and clearing affected global variables.
//!
//! \return None.
//
//===============================================================
void
TRF79xxA_reset(void)
{
TRF79xxA_sendDirectCommand(TRF79XXA_SOFT_INIT_CMD);
TRF79xxA_sendDirectCommand(TRF79XXA_IDLE_CMD);
MCU_delayMillisecond(1);
TRF79xxA_resetFIFO(); // Reset the FIFO
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x01); // ASK 100%, no SYS_CLK output
TRF79xxA_writeRegister(TRF79XXA_REGULATOR_CONTROL, 0x01);
#if (TRF79xxA_VERSION == 70)
TRF79xxA_writeRegister(TRF79XXA_NFC_TARGET_LEVEL, 0x00); // For TRF7970A Errata
#endif
#if (TRF79xxA_VERSION == 70)
g_eTrfGeneralSettings.ui8IsoControl = 0x21;
#elif (TRF79xxA_VERSION == 60)
g_eTrfGeneralSettings.ui8IsoControl = 0x02;
#endif
g_eTrfGeneralSettings.bRfFieldOn = false;
g_ui8FifoOffset = 0;
g_ui8FifoRxLength = 0;
}
//===============================================================
//
//! TRF79xxA_resetIrqStatus - Resets the IRQ Status Register of
//! the TRF79xxA
//!
//! This function resets/clears the TRF79xxA IRQ Status Register
//!
//! \return None.
//
//===============================================================
void TRF79xxA_resetIrqStatus(void)
{
uint8_t puiIrqStatus[2];
puiIrqStatus[0] = TRF79XXA_IRQ_STATUS;
puiIrqStatus[1] = TRF79XXA_IRQ_MASK;
TRF79xxA_readContinuous(puiIrqStatus, 2); // read second reg. as dummy read
}
//===============================================================
//
//! TRF79xxA_turnRfOff - Turn off the transmission of the TRF79xxA
//! RF Field
//!
//! This function stops the TRF79xxA transmitting an RF field
//!
//! \return None.
//
//===============================================================
void TRF79xxA_turnRfOff(void)
{
uint8_t ui8Value;
ui8Value = g_eTrfGeneralSettings.eTrfPowerSetting;
TRF79xxA_writeRegister(TRF79XXA_CHIP_STATUS_CONTROL,ui8Value);
g_eTrfGeneralSettings.bRfFieldOn = false; // Update RF Field variable
}
//===============================================================
//
//! TRF79xxA_turnRfOn - Turns on the transmission of the TRF79xxA
//! RF Field
//!
//! This function enables the TRF79xxA transmit an RF field
//!
//! \return None.
//
//===============================================================
void TRF79xxA_turnRfOn(void)
{
uint8_t ui8Value;
ui8Value = g_eTrfGeneralSettings.eTrfPowerSetting | 0x20; // Turn RF field On
TRF79xxA_writeRegister(TRF79XXA_CHIP_STATUS_CONTROL,ui8Value);
g_eTrfGeneralSettings.bRfFieldOn = true; // Update RF Field variable
}
//===============================================================
//
//! TRF79xxA_writeContinuous - Write to consecutive TRF79xxA
//! registers.
//!
//! \param pui8Payload is the address of the first register
//! followed by the contents to write for each register
//! \param ui8Length is the number of registers to write + 1
//! Minimum value of ui8Length allowed = 2 (a write to 1 register)
//!
//! This function writes data to a specific number of TRF79xxA
//! registers from a specific address.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_writeContinuous(uint8_t * pui8Payload, uint8_t ui8Length)
{
if (ui8Length > 1) // Cannot specify a length of 1
{
if (*pui8Payload == TRF79XXA_CHIP_STATUS_CONTROL) // If the write starts at the Chip Status Control Register
{
if (((*pui8Payload+1) & BIT5) == BIT5) // Check for RF field bit and update variable
{
g_eTrfGeneralSettings.bRfFieldOn = true;
}
else
{
g_eTrfGeneralSettings.bRfFieldOn = false;
}
if (ui8Length > 2) // Check if the write length includes the ISO Control Register being written to (0x01)
{
g_eTrfGeneralSettings.ui8IsoControl = (*pui8Payload+2); // If so, update the Iso Control Register variable
}
}
else if (*pui8Payload == TRF79XXA_ISO_CONTROL) // If the write starts at the ISO Control Register
{
g_eTrfGeneralSettings.ui8IsoControl = *pui8Payload+1; // Update the ISO Control Register variable
}
// Call continuous write function
SPI_writeCont(pui8Payload, ui8Length);
}
else
{
// Error, cannot specify a length of 1
return;
}
}
//===============================================================
//
//! TRF79xxA_writeRegister - Write single to a TRF79xxA Register
//!
//! \param ui8TrfRegister is the register address for the write
//! \param ui8Value is the value to write to the specified
//! register
//!
//! This function writes a new value into a single TRF79xxA
//! register.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_writeRegister(uint8_t ui8TrfRegister, uint8_t ui8Value)
{
uint8_t pui8Write[2];
if (ui8TrfRegister == TRF79XXA_ISO_CONTROL)
{
// Attempt to enable Card Emulation/Peer to Peer which is not supported by firmware
// Exit function to avoid issues with that
if ((ui8Value & BIT5) == BIT5)
{
return;
}
g_eTrfGeneralSettings.ui8IsoControl = ui8Value; // Update the ISO Control Register variable
}
if (ui8TrfRegister == TRF79XXA_CHIP_STATUS_CONTROL)
{
if ((ui8Value & BIT5) == BIT5) // Check for RF field bit and update variable
{
g_eTrfGeneralSettings.bRfFieldOn = true;
}
else
{
g_eTrfGeneralSettings.bRfFieldOn = false;
}
}
pui8Write[0] = ui8TrfRegister;
pui8Write[1] = ui8Value;
SPI_writeSingle(pui8Write);
}
//===============================================================
//
//! TRF79xxA_setupInitiator - Write the initial settings for
//! a set of TRF79xxA registers based on which protocol is to be
//! enabled.
//!
//! \param ui8IsoControl is the value to write to the ISO Control
//! register of the TRF79xxA
//!
//! This function is used to configure a series of TRF79xxA
//! registers based on which RFID technology will be enabled in
//! the ISO control register.
//!
//! This function will only enables one RFID technology at a time.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_setupInitiator(uint8_t ui8IsoControl)
{
TRF79xxA_reset(); // Reset the TRF7970A to ensure a clean state of operation before changing modes
TRF79xxA_turnRfOn(); // Turn on the RF field
g_eTrfGeneralSettings.ui8IsoControl = ui8IsoControl; // Update the ISO Control Register variable
// Register 0x01 - ISO Control Register
TRF79xxA_writeRegister(TRF79XXA_ISO_CONTROL,ui8IsoControl);
switch (ui8IsoControl)
{
case 0x08: // ISO14443A + RX CRC
case 0x88: // ISO14443A + no RX CRC
// Register 0x09 - System Clock Output, Modulation Scheme
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x01); // Sys Clock Output = 13.56MHz, OOK = 100%
#if (TRF79xxA_VERSION == 60) // Some 60A registers aren't initialized properly on ISO Control Writes (SLOA155, Section 7.8)
// Register 0x07 - No Response Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_NO_RESPONSE_WAIT_TIME, 0x0E);
// Register 0x08 - RX Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_WAIT_TIME, 0x07);
#endif
break;
case 0x0C: // ISO14443B
// Register 0x09 - System Clock Output, Modulation Scheme
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x00); // Sys Clock Output = 13.56MHz, ASK 10%
#if (TRF79xxA_VERSION == 60) // Some 60A registers aren't initialized properly on ISO Control Writes (SLOA155, Section 7.8)
// Register 0x07 - No Response Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_NO_RESPONSE_WAIT_TIME, 0x0E);
// Register 0x08 - RX Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_WAIT_TIME, 0x07);
#endif
break;
case 0x02: // ISO15693
// Register 0x09 - System Clock Output, Modulation Scheme
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x01); // Sys Clock Output = 13.56MHz, OOK = 100%
// Resgister 0x07 - No Response Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_NO_RESPONSE_WAIT_TIME, 0x15);
#if (TRF79xxA_VERSION == 60) // Some 60A registers aren't initialized properly on ISO Control Writes (SLOA155, Section 7.8)
// Register 0x08 - RX Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_WAIT_TIME, 0x1F);
#endif
break;
case 0x1A: // FeliCa 212kbps
case 0x1B: // FeliCa 424kbps
// Register 0x09 - System Clock Output, Modulation Scheme
TRF79xxA_writeRegister(TRF79XXA_MODULATOR_CONTROL, 0x00); // Sys Clock Output = 13.56MHz, ASK 10%
#if (TRF79xxA_VERSION == 60) // Some 60A registers aren't initialized properly on ISO Control Writes (SLOA155, Section 7.8)
// Register 0x07 - No Response Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_NO_RESPONSE_WAIT_TIME, 0x0E);
// Register 0x08 - RX Wait Time
TRF79xxA_writeRegister(TRF79XXA_RX_WAIT_TIME, 0x01);
#endif
break;
default:
break;
}
#if (TRF79xxA_VERSION == 70)
// Register 0x14 - Adjustable FIFO Level
TRF79xxA_writeRegister(TRF79XXA_FIFO_IRQ_LEVELS, 0x0C);
// Register 0x18 - NFC Target Detection Level
// This register must be written to 0x00 per TRF7970A Errata
TRF79xxA_writeRegister(TRF79XXA_NFC_TARGET_LEVEL, 0x00);
#endif
}
//===============================================================
//
//! TRF79xxA_waitTxIRQ - Timeout sequence for just TX
//!
//! \param ui8TxTimeout is the TX timeout in milliseconds
//!
//! This function ensures data has been transmitted correctly
//! only.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_waitTxIRQ(uint8_t ui8TxTimeout)
{
g_sTrfStatus = RX_WAIT;
g_ui8TimeoutFlag = 0x00;
while((g_sTrfStatus != TX_COMPLETE) && (g_sTrfStatus != TX_ERROR))
{ // Wait for end of TX
// Clear the IRQ Flag
g_ui8IrqFlag = 0x00;
// Setup for the Timer
MCU_setCounter(ui8TxTimeout);
while((g_ui8IrqFlag == 0x00) && (g_ui8TimeoutFlag == 0x00)) // Wait for an interrupt
{
// Do Nothing
}
RESET_COUNTER;
if (g_sTrfStatus != TX_COMPLETE)
{
if (g_sTrfStatus == TX_WAIT) // Wait longer since we received an 0xA0
{
TRF79xxA_waitTxIRQ(ui8TxTimeout); // Wait longer for transmission to complete
}
else // Failed to send packet properly - Exit TX Timeout
{
g_sTrfStatus = TX_ERROR; // Set status to error
}
}
}
}
//===============================================================
//
//! TRF79xxA_waitRxIRQ - Timeout sequence for just RX
//!
//! \param ui8RxTimeout is the RX timeout in milliseconds
//!
//! This function determines if any data has been received prior
//! to the RX timeout only.
//!
//! When the RX timeout occurs before data is received, then mark
//! the TRF79xxA status as a No Response Received status.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_waitRxIRQ(uint8_t ui8RxTimeout)
{
g_ui8FifoOffset = 0; // Reset the FIFO Offset prior to receiving data
g_sTrfStatus = RX_WAIT;
g_ui8TimeoutFlag = 0x00;
while(g_sTrfStatus == RX_WAIT) // Wait for end of RX or timeout
{
// Clear the IRQ Flag
g_ui8IrqFlag = 0x00;
// Setup for the Timer
MCU_setCounter(ui8RxTimeout);
while((g_ui8IrqFlag == 0x00) && (g_ui8TimeoutFlag == 0x00)) // Wait for an interrupt
{
// Do Nothing
}
while (g_sTrfStatus == RX_WAIT_EXTENSION)
{
g_ui8IrqFlag = 0x00;
#if (TRF79xxA_VERSION == 70)
if ((g_eTrfGeneralSettings.ui8IsoControl & 0x1F) > 0x07)
{
MCU_setCounter(7);
}
else
{
MCU_setCounter(50);
}
#endif
#if (TRF79xxA_VERSION == 60)
MCU_setCounter(5);
#endif
while((g_ui8IrqFlag == 0x00) && (g_ui8TimeoutFlag == 0x00)) // Wait for an interrupt
{
// Do Nothing
}
#if (TRF79xxA_VERSION == 60)
if (g_sTrfStatus == NO_RESPONSE_RECEIVED)
{
g_sTrfStatus = RX_COMPLETE;
}
#endif
}
RESET_COUNTER;
if (g_sTrfStatus == RX_WAIT)
{
// Exit the while loop
g_sTrfStatus = NO_RESPONSE_RECEIVED;
}
}
}
//===============================================================
//
//! TRF79xxA_waitRxData -
//!
//! \return g_sTrfStatus returns the current TRF79xxA drive
//! status
//
//===============================================================
tTrfStatus TRF79xxA_waitRxData(uint8_t ui8TxTimeout, uint8_t ui8RxTimeout)
{
switch (g_sTrfStatus)
{
case TRF_IDLE:
case TX_WAIT:
TRF79xxA_waitTxIRQ(ui8TxTimeout); // TX timeout
TRF79xxA_waitRxIRQ(ui8RxTimeout); // RX timeout
break;
case TX_COMPLETE:
TRF79xxA_waitRxIRQ(ui8RxTimeout); // RX timeout
break;
case NO_RESPONSE_RECEIVED_15693:
// Do Nothing
break;
case COLLISION_ERROR:
if ((g_eTrfGeneralSettings.ui8IsoControl == 0x02) || (g_eTrfGeneralSettings.ui8IsoControl == 0x08) || (g_eTrfGeneralSettings.ui8IsoControl == 0x88))
{
// Do Nothing
}
else
{
return g_sTrfStatus;
}
break;
case RX_COMPLETE:
case RX_WAIT:
case RX_WAIT_EXTENSION:
// Do Nothing
break;
default:
g_sTrfStatus = TX_ERROR;
break;
}
return g_sTrfStatus;
}
//===============================================================
//
//! TRF79xxA_getTrfStatus - Returns current TRF79xxA driver
//! status
//!
//! \return g_sTrfStatus returns the current TRF79xxA drive
//! status
//
//===============================================================
tTrfStatus TRF79xxA_getTrfStatus(void)
{
return g_sTrfStatus;
}
//===============================================================
//
//! TRF79xxA_setTrfStatus - Set the TRF79xxA driver status
//!
//! \param sTrfStatus is the new TRF79xxA driver status
//!
//! This function sets the TRF79xxA driver status manually.
//! This can be used to modify the TRF driver status without an
//! IRQ event. Use with caution.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_setTrfStatus(tTrfStatus sTrfStatus)
{
g_sTrfStatus = sTrfStatus;
}
//===============================================================
//
//! TRF79xxA_setTrfPowerSetting - Set the TRF79xxA power setting
//!
//! \param sTrfPowerSetting is the new TRF79xxA Power Setting
//!
//! This function allows for configuration of the TRF79xxA power
//! setting.
//!
//! Options are:
//! - TRF79xxA_3V_FULL_POWER: 3V TRF79xxA input w/ full power RF output
//! - TRF79xxA_5V_FULL_POWER: 5V TRF79xxA input w/ full power RF output
//! - TRF79xxA_3V_HALF_POWER: 3V TRF79xxA input w/ half power RF output
//! - TRF79xxA_5V_HALF_POWER: 5V TRF79xxA input w/ half power RF output
//!
//! \return None.
//
//===============================================================
void TRF79xxA_setTrfPowerSetting(tTrfPowerOptions sTrfPowerSetting)
{
g_eTrfGeneralSettings.eTrfPowerSetting = sTrfPowerSetting;
}
//===============================================================
//
//! TRF79xxA_getCollisionPosition - Return the current Collision
//! Position value
//!
//! This function will return the current Collision Position
//! value.
//! This is only used for the ISO14443 Type A anti-collision
//! process.
//!
//! \return g_ui8CollisionPosition returns the current Collision
//! Position value
//
//===============================================================
uint8_t TRF79xxA_getCollisionPosition(void)
{
return g_ui8CollisionPosition;
}
//===============================================================
//
//! TRF79xxA_setCollisionPosition - Set the Collision Position
//! variable
//!
//! \param ui8ColPos is the new Collision Position value
//!
//! This function sets the Collision Position variable.
//! This is only used for the ISO14443 Type A anti-collision
//! process.
//!
//! \return None.
//
//===============================================================
void TRF79xxA_setCollisionPosition(uint8_t ui8ColPos)
{
g_ui8CollisionPosition = ui8ColPos;
}
//===============================================================
//
//! TRF79xxA_getRxBytesReceived - Returns the Number of RX Bytes
//! received by the TRF79xxA FIFO
//!
//! This function returns the number of bytes received by the
//! TRF79xxA during the last packet reception.
//!
//! This is used to check for how much data has been received
//! and to ensure packets with expected lengths were fully
//! received.
//!
//! \return g_ui8FifoRxLength returns the current FIFO RX Length
//
//===============================================================
uint8_t TRF79xxA_getRxBytesReceived(void)
{
return g_ui8FifoRxLength;
}
//===============================================================
//
//! TRF79xxA_getTrfBuffer - Returns a point to the start of the
//! TRF Buffer.
//!
//! This function will return a pointer for the start address of
//! the TRF79xxA Data Buffer.
//!
//! This is used to access the data received from successful RF
//! commands in files which do not have naturally have access to
//! the g_pui8TrfBuffer.
//!
//! \return &g_pui8TrfBuffer[0] returns the start address of
//! g_pui8TrfBuffer.
//
//===============================================================
uint8_t * TRF79xxA_getTrfBuffer(void)
{
return &g_pui8TrfBuffer[0];
}
//===============================================================
//
//! TRF79xxA_getIsoControlValue - Fetch the latest Iso Control
//! Register value
//!
//! This function returns the current TRF79xxA ISO Control
//! Register setting .
//!
//! The ISO Control Register value is updated whenever a read or
//! write to the ISO Control Register occurs.
//!
//! \return g_ui8IsoControlValue returns the current ISO Control
//! Register value
//
//===============================================================
uint8_t TRF79xxA_getIsoControlValue(void)
{
return g_eTrfGeneralSettings.ui8IsoControl;
}
//===============================================================
//
//! TRF79xxA_checkExternalRfField - Checks if an external RF field
//! is present.
//!
//! This function performs RF collision avoidance as outlined in
//! TI application notes (sloa192, sloa227) in order to determine
//! if an external RF field is present.
//!
//! \return bExtFieldOn retuns the external RF field status
//
//===============================================================
bool TRF79xxA_checkExternalRfField(void)
{
bool bExtFieldOn;
uint8_t ui8Value;
TRF79xxA_writeRegister(TRF79XXA_CHIP_STATUS_CONTROL, 0x02);
TRF79xxA_sendDirectCommand(TRF79XXA_TEST_EXTERNAL_RF_CMD);
__delay_cycles(400); // Delay for 50uS
ui8Value = TRF79xxA_readRegister(TRF79XXA_RSSI_LEVELS);
if ((ui8Value & 0x07) > 1) // Check for RF field bit and update variable
{
bExtFieldOn = true;
}
else
{
bExtFieldOn = false;
}
return bExtFieldOn;
}
//===============================================================
//
//! TRF79xxA_timerHandler - Handler for assigned MCU Timer
//! Interrupt of TX/RX Timeout functions.
//!
//! This function processes the Timer Interrupt for the TX/RX
//! timeout functions. If a timeout occurs, the IRQ Status
//! register is read out to determine the current TRF79xxA state.
//!
//! \return None.
//
//===============================================================
#pragma vector=TIMER0_A0_VECTOR
__interrupt void
TRF79xxA_timerHandler(void)
{
uint8_t ui8IrqStatus;
STOP_COUNTER;
g_ui8TimeoutFlag = 0x01;
ui8IrqStatus = TRF79xxA_readIrqStatus();
if(ui8IrqStatus == TRF79XXA_IRQ_STATUS_TX_COMPLETE)
{
g_sTrfStatus = TX_COMPLETE;
}
else if(ui8IrqStatus == TRF79XXA_IRQ_STATUS_IDLE)
{
g_sTrfStatus = NO_RESPONSE_RECEIVED;
}
else
{
g_sTrfStatus = RX_WAIT;
}
}
//===============================================================
//
//! TRF79xxA_irqHandler- Interrupt handler for IRQ interrupts
//!
//! Handles receiving IRQ's, getting IRQ status, and maintaining
//! timers/global variables
//!
//! \return None.
//
//===============================================================
#pragma vector = PORT2_VECTOR
__interrupt void
TRF79xxA_irqHandler(void) // interrupt handler
{
uint8_t ui8IrqStatus;
STOP_COUNTER; // stop timer mode
g_ui8IrqFlag = 0x01;
do
{
IRQ_CLR; // PORT2 interrupt flag clear
// IRQ status register has to be read
ui8IrqStatus = TRF79xxA_readIrqStatus();
if(ui8IrqStatus == 0xA0) // TX active and only 3 bytes left in FIFO
{
g_sTrfStatus = TX_WAIT;
break;
}
else
{
TRF79xxA_processIRQ(&ui8IrqStatus);
}
} while((IRQ_PORT & IRQ_PIN) == IRQ_PIN);
__bic_SR_register_on_exit(LPM0_bits);
}
//*****************************************************************************
//
// Close the Doxygen group.
//! @}
//
//*****************************************************************************
What modification needs to be applied to use TRF7960A?
Customer checked section 4.1 in below FAQ for software modification, but these changes are already done in TI code.
https://www.tij.co.jp/jp/lit/an/sloa248b/sloa248b.pdf
Thanks and regards,
Koichiro Tashiro