I have the TRF7960EVM and have been using it and its integrated coil antenna to transfer power to a parallel resonant circuit, which is just an unshielded inductor and tuning cap with Schottky diode. With the EVM I just plug it into USB and I can see it immediately at 13.56 MHz on the spectrum analyzer. For my application I am just putting the EVM in proximity to the receive circuit to charge a large electrolytic capacitor (2mF) which will power a very low power MSP430 for a few seconds. My question is how I might go about using the TRF7960 for this application. I will be doing no actual RFID data transmission I just want the TRF7960 to output power to the resonant circuit. What does the TRF7960 do upon startup if no microcontroller communicates with it?