This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: target mode - card emulation

Part Number: TRF7970A


Hello team,

I have tried a lot, read a lot.. but I didn't get card emulation with TRF7970a running.

I use a DLP booster pack on a custom board and ported the TI NFC stack.

Reading a iso15693 tag works so I think my communcation with TRF seems to be ok.

But in target mode only strange things happen.
If I try to read my emulated tag via smartphone I get rx complete interrupts from TRF.
The received data looks like garbage and "TRF79x0_targetInitialize" fails.

I see fifo contents like "06 00 ff ff 01 00" and "00 00 00" which the stack can not handle.

Is there a way to check what is done during first negotitation between smartphone and TRF?
For me it looks like a misinterpreting.

cheers
Mathias

  • Hi Matthias,

    at first one question, which tag type do you want to emulate?

    Regarding the smartphone I don't know which sequence is send to detect which tag type is in the field. I would recommend to use your DLP booster pack with the EXP430F5529LP Launchpad together with our NFC demo software. You could then trace the SPI communication with a logic analyzer to get a reference for your development.

    Best Regards,

    Helfried

  • Hi Matthias,

    I haven’t heard back from you for a while, so this tread is being closed. If you wish to continue the discussion, please post a reply with an update below (or create a new thread).

    Best Regards,
    Helfried