Other Parts Discussed in Thread: RF-HDT-DVBE, RF-HDT-DVBB
These TI Tag-It RFID inlays have gone EOL.

Is this TI part its closest replacement: RF37S114 Tag-it HF-I Type 5 NFC, ISO/IEC 15693 Transponder, 4 mm × 4 mm
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
These TI Tag-It RFID inlays have gone EOL.

Is this TI part its closest replacement: RF37S114 Tag-it HF-I Type 5 NFC, ISO/IEC 15693 Transponder, 4 mm × 4 mm
Hi Scott,
TI has stopped selling inlay transponders like the one on your picture and is concentrated on selling only the chips to the inlay manufacturer.
There a 3 transponders available, one is the RF37S114 which is very small with a size of 4mm x 4mm. The other two are round over-molded types with a diameter of ~2cm (RF-HDT-DVBB, RF-HDT-DVBE).
All of these are ISO15693 compliant but complete different in size to the transponder you are looking for.
Best Regards,
Helfried