This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: DSSS at 2.4GHz

Part Number: CC1352R
Other Parts Discussed in Thread: SYSCONFIG

Hi,

Customers are developing based on the CC1352R and EasyLink Example.

sysconfig PHY settings


Customers want to use 250kbps DSSS at 2.4GHz.
When set to 2400MHz, DSSS cannot be found in PHY Type.

Is it possible with this device?

CC1352R
SmartRF Studio7 2.13.0
Sysconfig 1.6.0
SimpleLinkTm CC13x2_26x2 SDK 4.30.00.54

Best regards,

Rei