I am using some Anaren A1101R09A modules for a project I am working on. I am using their pre-certified 1.2kbaud 2-FSK setup, so I know the configurations are accutate for the 915MHz setup. I have a dedicated LDO for the modules and followed the ground plane requirements per Anaren's specs. This modules have the built in 2dBi antenna, so that should take some of the guesswork out (though it means that I cannot disconnect it. While doing some line of site testing with the module on tripods, I seemed to get pretty poor results. I sent a 7 byte packet every 4 seconds and looked at the RSSI and LQI values every 50 feet. My results where:
|
Distance (LOS) |
LQI |
RSSI |
Notes |
|
100ft |
0 – 1 |
-67 – -68 |
|
|
150ft |
6 – 23 |
-74 – -75 |
|
|
200ft |
127 |
-78 – -80 |
|
|
250ft |
125 – 127 |
-80 – -83 |
Had a few 84s and 100s for LQI mixed in |
|
300ft |
127 |
-80 |
|
|
350ft |
126 – 127 |
-86 – -89 |
Had a CRC error |
|
400ft |
127 |
-86 – -89 |
|
|
450ft |
121 – 127 |
-85 – -90 |
|
|
500ft |
104 – 127 |
-95 – -100 |
LQIs bouncing around a lot; numerous CRC errors at this distance |
I am a little confused why the LQI would fall off the end of the table like that, and the RSSIs would be more linear. I thought that using the low datarate with the built-in 2dBi antennas with 2-FSK would have gotten me MUCH better distances.
Any ideas how I can vet this further?