Other Parts Discussed in Thread: SYSCONFIG,
Hello,
I'm currently experimenting with different protocols in the 2.4 GHz and Sub-1-Ghz Band. I'd like to experiment with the TI 15.4 stack in the 2.4 GHz band.
I've downloaded the collector/sensor example from the SimpleLink CC13xx CC26xx SDK 5.40.00.40. But in the SysConfig tool, I can't change the frequency band to 2.4 GHz . The description of the option says:
The TI 15.4 Stack can be configured for operation in Sub-1 GHz and 2.4GHz frequency bands.
Default: The frequency band selected in this project is automatically configured based on the example. Please see the other examples provided in the SDK if another frequency band is desired.
Unfortunately, I cannot find the mentioned example and I don't know what is meant by "other examples of the SDK".
So my questions are:
- Is there an example for the TI 15.4 Stack working on the 2.4 GHz band? If yes, where can I find it?
- If there's no such example, can I change the given example to my desired frequency band and how?
Any help would be appreciated. Thank you in advance.
Alex