Other Parts Discussed in Thread: CC2652P, SYSCONFIG,
Hi,
I know it was asked multiple times in the forum, but most of these threads are older so I hope this feature was made usable in the meantime or there is a workaround.
I want to test the range of the CC1352P in the 2.4 GHz band in proprietary mode. Naturally, I would also like to test it with a high transmission power.
This thread states that the high PA can be activated in the 802.15.4 mode, but in my case, even this is not possible (with Smart RF Studio 7 ver 2.24.0). The thread that was linked to states that you can add pOverridesTx20[] and the txPowerTable into the RF configuration via the Code Export Tool of SmartRF Studio when choosing the BLE mode of the CC2652P with 20 dBm (it revolves around the CC2652P, though). When I use the pOverridesTx20 from there, the CC1352P seems to use a very low transmission power setting (the RSSI is about -68 dBm for another LaunchPad that lies directly next to the Transmitter, compared to -15 dBm when using 5 dBm transmission power). The same happens if I use the pOverrideTx20 from the 802.15.4 mode of the CC2652P.
Is the High PA still not available in 2.4 GHz proprietary mode? And is there a workaround for at least evaluating the range in the frequency band for our application?
Thank you in advance.
Alex