This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EPC Generation2 using CC1110

Hi

 

I want to build up an active RF-ID tag System using CC1110. So we wanted to use the protocol in it is EPC Generation 2 R/W, Full Anti-collision, DRM.

Tag standard is ISO/IEC 18000-6C and operating frequency 840-960Mhz

Please help me in having source code or hex files to generate this standard and accept them in reader to use them.

 

Advance Thanks and Regards,

Sai Jagini