This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: Board Troubleshooting

Part Number: LAUNCHXL-CC1352R1
Other Parts Discussed in Thread: CC1350, ENERGIA

Hi Team, need some assistance troubleshooting

Used "energia-1.8" IDE with EasyLink library v.1.0.4  for CC13xx boards.
Selected "Launchpad w/ cc1350 EMT(48 MHz)" on the menu.
There were two COM-ports and I selected one which wasn't uart.
After that opened one of the examples "blink" and tried to compile it.
Saw that red programmer LED blinked once and after that my PC doesn't see COM-port of LaunchPad board.

Thank you.

-Mark