Hi my name is Matias Lao, I'm currently using 2 LP-CC1352P7-4 and running the rfEcho example projects (Tx and Rx respectively).
I've modified the default custom RF Stack settings to use 'Custom PHY Setting, 2400 Mhz band' instead. The modified runs and shows the expected behavior on both Tx and Rx devices.
Next step was to use the high PA RF path to increase output power and extend the RF range.
However, after enabling the setting, compiling the code and programming the CC1352P7, the device stopped responding as expected. Neither the green nor red LEDs are blinking.
Is there any restriction for the configuration being used or any knwon issue?
Thanks in advance,
Matias