This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3404MR/NOPB



在12V输入时,能快速启动带动9V/3W的LED负载,不会出现启动时LED闪烁的情况,这个正常,

但是在输入14V或更高时,启动时输出不稳定,导致LED闪烁,有时甚至无法带动9V/3W负载。

在低温-5℃时,输入12V/14V都无法启动,无法使得LED点亮

在低温-5℃时,输入12V/14V都无法启动,无法使得LED点亮,这是目前的主要问题点,我们在输入部分直接通过DC SUPPLIY 供电给IC( PIN8& GND),

此IC 仍然不能工作