Hi all,
I've been developing hardware based on the CC1110 reference design. However, when I check the radio output signal on a spectrum analyser, the frequency is offset from the value set in the register, by about 150kHz. This offset is systematic (does not very with frequency). I've compared it with a CC1110 eval module on a SRF04 board, and found no offset occurs - the demo board setup transmits at exactly the programmed frequency (I'm transmitting at 434 MHz).
Can anyone think of an obvious reason why this offset might occur?