Other Parts Discussed in Thread: MSP-FET,
Hi Experts,
Our customer is trying to program the RF430FRL152H chip by its EVM JTAG schematic but wonders if the power3V3 is needed
He came across a question in the forum saying that is unnecessary
e2e.ti.com/.../level-shifter-for-jtag-from-fet-to-rf430frl152-with-sn74lvc2g125-and-sn74auc1g04
He is asking what is he supposed to do if it is unnecessary? like connect it to the ground or just connect nothing?
and another question is if these so-called necessary caps and resistors are needed when programming.
what the customer focuses on is the JTAG module and especially for the POWER_3V3. He thought there are 3 possibilities: perceive it as MSP_VCC and connect it to JTAG pin2/connect it to nothing(then 2 relevant resistors R32 and R34 can be removed as well)/connect it to GND. and then it doesn't give the answer if the necessary caps and resistors are needed when programming the chip. He said: "i must declare that all i am intending to do now is to burn the chip successfully"
The customer also said "the power_3v3 is sure to be unnecessary for programming since it comes from the USB power supply(you can confirm this from the power section schematics in the user guide), and we don't need to connect the EVM to the USB while programming the EVM by MSP-FET(also be confirmed in the user guide ). What I need to know is how should I handle this to ensure that I can burn the chip successfully"
And to make sure the customer can program the chip he also need to know if the external components are required when programming(see in RF430FRL15xH FAQ file 2.3)
e2e.ti.com/.../rf430frl152h-troubles-connecting-programming-via-jtag
it seems that this guy has added the external components to burn the chip
We hope to hear your advice. Thank you so much in advance.
Kind regards,
Gerald