Other Parts Discussed in Thread: MSP-EXP430G2ET, DLP-7970ABP
Hi Andreas,
I received the LaunchPad (MSP-EXP4302ET) and am able to load an run the TRF7970ABP_RFID_Reader_Demo code, but it does read any tags.
The code seems to be stuck at this line:
void TRF79xxA_waitTxIRQ(uint8_t ui8TxTimeout)
{
g_sTrfStatus = RX_WAIT;
g_ui8TimeoutFlag = 0x00;
while((g_sTrfStatus != TX_COMPLETE) && (g_sTrfStatus != TX_ERROR))
{ // Wait for end of TX
// Clear the IRQ Flag
g_ui8IrqFlag = 0x00;
// Setup for the Timer
MCU_setCounter(ui8TxTimeout);
while((g_ui8IrqFlag == 0x00) && (g_ui8TimeoutFlag == 0x00)) // Wait for an interrupt
{
// Do Nothing
}
RESET_COUNTER;
if (g_sTrfStatus != TX_COMPLETE)
{
......
Maybe I need to do something on the launchpad with one of the jumpers or something?
Thanks,
Becky