I am trying to connect a 4-wire load cell to the the CC26X2R1 to use the ADC. In Sensor Controller Studio, how do I configure the pin layout for a sensor (the load cell) that has a differential analog output (meaning I need a differential input to the CC26X2R1)? The "adcSelectGpioInput" only has parameters for 1 pin, and the only differential option I see is for a differential output.
If differential input is not possible, do you have a recommended signal conditioner or other hardware (preferably with amplifier) to sit between the load cell and the CC26X2R1? Thanks!
Link to the load cell datasheet: www.farnell.com/.../2849896.pdf