Dear All,
DN119 describes using P0_7 as an input pin to perform asynchronous serial transfer of radio signal.
How can I apply the same technology in CC1111 where P0_7 is not there?
Thanks,
Tony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
DN119 describes using P0_7 as an input pin to perform asynchronous serial transfer of radio signal.
How can I apply the same technology in CC1111 where P0_7 is not there?
Thanks,
Tony
// 4) Make P0.7 becomes Serial Data Input in TX mode by configuring the pin to have
// peripheral function
P0SEL.SELP0_[7] = 1; // This configures the pin to periperal mode
Page 96/244 shows the function of P0SEL but the data sheet including Table 50 is otherwise silent on this pin as a serial input or how to re-map it to another pin. I believe this is an artifact of a "Reserved" PKTCTRL0 being used that is otherwise undocumented. Ti will have to help on this one.