Hello,
I have the stellaris robotic evaluation board and I have put the CC 2530 EM module on the wireless socket.
I would like connect these two module using the SPI link. But on the schematics for the EVALBOT board I I don't understand what are the son connected to port H (pin 2 and 3).
Can you tell me if I must use the son of the port H, pin 2 and 3, for the SPI link.
Sorry for my English, I am a French student.
regards.
Vincent GARAVIlLON