Hello,
I'm putting together a simple test fixture to measure the RF power from a device under test (DUT) which is a TI LPRF module. It will be transmitting RF carrier at a given frequency, e.g. 2435MHz or so depending on the channel. Can I use any of the TI dev kits and firmware to verify that the output power is what we expect? I figure I just need to get the other chip (like a CC2520 or CC2500) to measure RF on one channel. How do I do this? Preferably a LPRF IC that connects to an MSP430.
Thanks,
Derek