I am trying to select the best micro-processor/RF transceiver for a wireless sensor application. I think the CC2510 is the closest to what I need, but I would like to hear what others have to say.
The rough specifications are as follows:
Min. Baud rate 125kbps, A/D 12 bits, Operating temperature ≈100 °C, Supply 3 V, Transmit current ≈12ma, Sleep current ≈0.7µA, Active Mode ≈300µA, Off Mode (RAM retention) ≈0.1µA, Number of Motes 256+, Wake-up Receive is highly desirable, RF 1 to 2.4GHz, Package area 10x10mm max.
Low power is very important since an energy harvester is used to supply power to the motes. I know that the transmit mode for the CC2510 is 17mA, but I am willing to accept this if the overall system power is low and the board area is small. Is there a better choice than the CC2510?