Hello,
I'm going to use Li-Ion cell for powering my device with chip CC111x. In datasheet I see that proper maximum VCC is 3.6V (absolute maximum is 3.9V), but Li-Ion can produce up to 4.2V. So it's impossible to connect CC111x to the battery directly. Of course I can use LDO linear regulator for this but it increases device's cost - it is critical in my case. So I have an idea - connect CC111x to the battery through silicon diode (in forward direction). It "eats" about 0.4V or more and VCC will be in permissible range. I'm sure the idea will work when CC111x is in active mode but what it will be in sleep when CC111x is comletely off? I mean if VCC is not more than 3.9V in this case?
Thanks in advance,
Alexey