There are two CC2511 modules on hand, one serving as the sending end and the other as the receiving end. The sending end sends a data packet after receiving the data sent by the serial port. Now both the sending end's (RFTXRXIF) and (IRQ-DONE) can be set normally, and it should be sending data normally, but the receiving end still cannot receive data. The receiving flag has been unresponsive. The receiving end has written a loop that always detects data. The first part below is the sending code, and the second part is the receiving (receiving did not perform data processing, only wrote the receiving flag detection). Could you please help me take a look? Thank you very much.
In addition, when the interrupt is enabled, the sending flag will not be set, and only when the interrupt is not enabled can the setting be sent normally.
void RF_Send_Init(void)
{
RFST=0x04;
IOCFG2=0X2E;
IOCFG0=0X06;
PKTCTRL0=0X05;
FSCTRL1=0X0A;
FREQ2=0X65;
FREQ1=0X60;
FREQ0=0X00;
MDMCFG4=0X76;
MDMCFG3=0XA3;
MDMCFG2=0X13;
MDMCFG1=0X23;
MDMCFG0=0X11;
DEVIATN=0X45;
MCSM0=0X14;
FOCCFG=0X16;
FSCAL1=0X00;
FSCAL0=0X11;
TEST1=0X31;
TEST0=0X09;
PA_TABLE0=0XFE;
RFST=0x04;
RFST=0x01;
while(MARCSTATE != 0x01);
RFTXRXIF=0;
}
void RF_Send(void)
{
unsigned char i=0;
RFST=0x04;
RFST=0x01;
while(MARCSTATE!=0x01);
RFTXRXIF=0;
RFTXRXIE=0;
RFIF &= ~0x10;
RFST=0x03;
while(!RFTXRXIF);
RFTXRXIF=0;
RFD=3;
for(i=0;i<3;i++)
{
while(!RFTXRXIF);
RFTXRXIF=0;
RFD=0x66;
}
while(!(RFIF & 0x10));
RFIF &= ~0x10;
}
void RF_Receive_Init(void)
{
RFST=0x04;
IOCFG2=0X2E;
PKTCTRL0=0X05;
FSCTRL1=0X0A;
FREQ2=0X65;
FREQ1=0X60;
FREQ0=0X00;
MDMCFG4=0X76;
MDMCFG3=0XA3;
MDMCFG2=0X13;
MDMCFG1=0X23;
MDMCFG0=0X11;
DEVIATN=0X45;
MCSM0=0X14;
FOCCFG=0X16;
FSCAL1=0X00;
FSCAL0=0X11;
TEST1=0X31;
TEST0=0X09;
PA_TABLE0=0XFE;
RFST=0x04;
RFST=0x01;
while(MARCSTATE != 0x01);
RFTXRXIF=0;
}
void RF_receive(void)
{
RFTXRXIF=0;
RFTXRXIE=0;
EA=1;
RFIF=RFIF& ~0x10;
RFST=0x02;
Usart0_Send_Onebyte(0x02);
while(!RFTXRXIF);
Usart0_Send_Onebyte(0x88);
}
After testing the RFIF flag, (IRQ_CS) will be set to 1 (automatically set to 1 in the next cycle after resetting). May I know when this flag bit will be generated?